Q
We design universal ISP programmers and need to develop a new algorithm for one
of our new programmers for ADuC7033. In the datasheet I can see that it is
programmable using the JTAG protocol. Is it possible for you to provide me the
programming specification of this device through this protocol? I ask you this
because the information that I can see from the datasheet are not enough for
our purposes.
If it is necessary we are available to sign an NDA document.
A
The JTAG interface on the ADuC7xxx is an industry standard JTAG port. Appended
is an incomplete application note that may be of help as a starting point.
Another option is to use the on-chip UART based bootloader. Details are
documented here:
https://www.analog.com/static/imported-files/application_notes/AN-724.pdf
The JTAG block is a functional block within the ARM7 core and the Debug Block
is described in detail in the ADM7TDMI Technical Reference Manual:
http://infocenter.arm.com/help/topic/com.arm.doc.ddi0210c/DDI0210B.pdf