ADUC7061
Production
The ADuC7060/ADuC7061 are fully integrated, 8 kSPS, 24-bit data acquisition systems incorporating high performance multi-channel sigma-delta (Σ-Δ) analog...
Datasheet
ADUC7061 on Analog.com
The data sheet says nothing about how these registers affect conversions. Is the value in the offset register subtracted from ADC results internally? If so, what is the scaling? Results are 24 bits, but the gain and offset registers are 16 bits. Is the gain calibration register used to internally modify the ADC conversions? If so, how? Is there a document that describes the process?
Hi,
The offset register is applied internally to the ADC results.
Similarly, the gain calibration register is applied internally scale the ADC results and minimize full scale errors.
Typically, the gain and offset errors are minimal, so a 16-bit register should suffice in correcting these errors.
Thanks,
Karl
Thanks for your reply, Karl.
I'm essentially reverse engineering a design of a colleague who has moved on. The issue is that the zero- and full-scale calibrations are being used to apply a gain and offset to a measurement. The zero value is not close to zero -- it's more like 10% of the reference voltage (~0.25V), and the full scale value is about 25% of the reference. My gut says this should cause scale and offset errors due to the resolution of the constants.
Ted