Hi ,
I am working on M355_ECSns_EIS example. For testing , 3 1K ohm resistors where connected in a star network and the resultant impedance shown was 1k in uart. Does this mean the evaluation board measures only one branch of star network ( between SE and star network midpoint) ? When 2K resistor was connected to SE and the midpoint of the star network, the impedance on uart was 2K Ohms. Could someone explain , what impedance ( between which points) is actually measured ?