Post Go back to editing

SPI transmission for ADUC7061

Thread Summary

The user inquires about transmitting 20 bytes of data using the SPI on the ADuC7xxx, which is designed for 8-bit transfers. The final answer confirms that the data must be loaded into the transmit FIFO and sent out 1 byte at a time, despite the 4-byte FIFOs. The thread is closed with an offer to post for further support if needed.
AI Generated Content
Product Number: aduc7061

Hi Team,

It seems that the SPI on the ADuC7xxx is designed for 8-bit transfers only. But there are 4-byte receive and transmit FIFOs.

So if 20bytes data is needed to transmit, will these data be needed to send 4 times?