Post Go back to editing

Aduc7023 program with USB-I2C/LIN CONV-Z

Category: Software
Product Number: Aduc7023, USB-I2C/LIN CONV-Z
Software Version: I2CFTWSD.exe

we want to use the USB-I2C_LIN-CONV-Z(MCV combi DONGLF) along with the I2CFTWSD.exe program to program Aduc7023. The driver of the "Aduc70xy USB-combi-Downloader" has been setup successfully.However, when running this program, it is unable to communicate with the aduc7023. there is a wrong message "couldn't find an FTDI device connected". How can I sovler this problem. Does it mean that the MCU(aduc7023 isn't connect to the USB-I2C_LIN-CONV-Z)

Parents
  • Hi,

    What is the operating system you are using? Are you using an evaluation board or your design already?

    Can you try the installer in the attached file? The installer should include the software: I2CWSD.

    MultiDongleSetup.zip

    Have you initiated the download mode entry sequence? I have attached a user guide, including a section about the I2C programming interface.

    You can try the I2CWSD and let me know if there are still any wrong messages.

    Thanks,
    Karl

  • How many times i can program the Aduc7023 with the USB-I2C/LIN conv-z? The hex file was burned into the MCU yesterday. But it isn't work whatever i try to program. The interface of the I2CWSD display "Timeout", It seems to inconnect with the Aduc7023. The 25 PIn (BM serial enable) is set “0” adcorrding to the user guide.  

Reply
  • How many times i can program the Aduc7023 with the USB-I2C/LIN conv-z? The hex file was burned into the MCU yesterday. But it isn't work whatever i try to program. The interface of the I2CWSD display "Timeout", It seems to inconnect with the Aduc7023. The 25 PIn (BM serial enable) is set “0” adcorrding to the user guide.  

Children