Dear Expert,
Customer use aduc7060 in project, Can aduc7060 be programmed through IAP(In Application Programming)?
If yes, can we share programming example code to customer?
Thanks a lot!
ADUC7060
Production
The ADuC7060/ADuC7061 are fully integrated, 8 kSPS, 24-bit data acquisition systems incorporating high performance multi-channel sigma-delta (S-?) analog...
Datasheet
ADUC7060 on Analog.com
Dear Expert,
Customer use aduc7060 in project, Can aduc7060 be programmed through IAP(In Application Programming)?
If yes, can we share programming example code to customer?
Thanks a lot!
Hi Robert,
I don't have experience using IAP to program aduc7060, but I did find an example of IAP working for aduc7020.
Implementing In-Application Programming on the ADuC702x | Analog Devices
I'm still reviewing if the example code applies to aduc7060 and if programming it through IAP is possible.
Hi Robert,
I confirmed that you could use the IAP example for ADuC7020 as a reference for implementing IAP on ADuC7060.
You should also consider that the flash of ADuC7060 is smaller than ADuC7020.
Regards,
Karl
魏老板 好,
客户尝试根据串行下载协议的内容,模仿ARMWSD,通过一块芯片给ADUC70XX升级。有以下几个问题:
1.ADUC70XX的内置微转换器(MicroConverter)接收的是否为hex格式的文件,是否需要对该文件进行处理再发送给ADUC70XX
2.ADUC70XX是否还需要编写相关程序来接受和处理升级文件
3.协议中规定了发送的数据包格式,其中地址字段(数据2至数据5)这一部分如何确定
4.ARMWSD是在计算机上的软件,有没有用C语言编写的发送代码
感谢感谢