Post Go back to editing

ADuC 7061 JLink "Cannot stop ARM device"

Keil mVision V15.4.0.0.  J-Link is default, not Chinese..

Something happened to the software and ADuC 7061 doesn't respond. Message JLink: "Cannot stop ARM device". Оn 6 chips. How can I erase the chips?



J-Link is default, not Chinese.
[edited by: AlexSAN at 2:31 PM (GMT -5) on 10 Feb 2022]
Parents
  • If you can't erase the chip in Keil, you can try using the ARMWSD downloader.

    You need to enter the serial download mode of the device. I attached a pdf that shows how to do so.

    When using the ARMWSD, the device communicates to the PC using UART, so you need a UART to USB cable. You will also need to use P1.0 and P1.1.

    ARMWSD.zip

    PDF

Reply
  • If you can't erase the chip in Keil, you can try using the ARMWSD downloader.

    You need to enter the serial download mode of the device. I attached a pdf that shows how to do so.

    When using the ARMWSD, the device communicates to the PC using UART, so you need a UART to USB cable. You will also need to use P1.0 and P1.1.

    ARMWSD.zip

    PDF

Children