Post Go back to editing

ADC problem about ADUC7061

I post this problem in chinese version, but the china engineer can't give correct answer. So i want to post it here to found an more senior engineer. 

As you know, ADC1~ADC5 are single function port. but ADC6~ADC9 are mutil-function prots.

The SPI/I2C and analog can be changed.

I write code to sample analog signle from ADC4 and ADC8, ADC 4 is connected to ADC8 together.

But when i read, value from ADC4 is correct, but data from ADC8 is not correct.

When the voltage is 0.67V around. the value from ADC4 is 0x004xxxxx, but value from ADC8 is about 0x000005xx.

When i change the voltage, value from ADC8 will not change, or chage slightly. for example, 0x5ff, 0x5fe.

When i change another device(CPU chip), the value will be 0x606, 0x607.

I  deduce:

there are some bug in device. and the codes to initiate ADC1 need special sequence.

the Datasheed does not tell me what is sequence, the special sequence, so i get wrong result.

I can't find example code how to use adc6~adc9,  will anyone give correct resolution?

thanks.

I post my code here:

int main()
{
volatile signed long s;
signed char N = -1;
char Err = 0;
float fN = 0;

PLLKEY1 = 0xaa;
PLLCON = 0x00;
PLLKEY2 = 0x55;

POWKEY1 = 0x1;
POWCON0 = 0x38; // Set core to max CPU speed of 10.24Mhz
POWKEY2 = 0xF4;

POWKEY3 = 0x76;
POWCON1 = 0x024;
POWKEY4 = 0xB1;

DACCON = 0x0013;
DACDAT = 0x04ff0000;


while(1)
{

ADCCFG = 0x84;
ADCFLT = 0x8083;

GP0CON0 = 0x00000000; //p0.0~p0.4 gpio
GP0PAR = 0x0f; //01110
GP0DAT = 0x10100000;

GP0KEY1 = 0x7;
GP0CON1 = 0x1; // adc
GP0KEY2 = 0x13;

ADC0CON = 0;
ADC1CON = 0x878c;;

s = ADCSTA;
s = ADC0DAT;
s = ADC1DAT;
//////////
ADCMDE = 0x83;
////
ADC1CON = 0x8004 | 0x0480;//ch 8
//ADC1CON = 0x800c | 0x0300;//ch 4

s = ADC1DAT;
s = ADCSTA;
ADCMDE = 0x82;
do
{
s = ADCSTA;
if (s & 0x2000) //adc1cerr
{
Err |= 1; //over range
}
} while(!(s & 0x2));

s = ADC1DAT;
ADCMDE = 0x83;

//3. exit adc
ADCMDE = 0x83; //idle
ADCFLT = 0x80ff;
ADC1CON = 0x78c; //internally shorted

GP0CON0 = 0x00001011; //back to spi
GP0PAR = 0x04;
GP0DAT = 0x10100000;

GP0KEY1 = 0x7;
GP0CON1 = 0x0; // exit adc
GP0KEY2 = 0x13;
}
}

Parents
  • Hi,

    You mentioned that CH4 is working while CH8 is not but looking at the configuration below, there is another difference. You bypass both buffer when reading from CH4. Can you try to bypass the buffer when using CH8 as well? This is just to check if we have an issue with the buffer. 

    ADC1CON = 0x8004 | 0x0480;//ch 8
    //ADC1CON = 0x800c | 0x0300;//ch 4

    Also, I think the lines below can be skipped.

    GP0CON0 = 0x00000000; //p0.0~p0.4 gpio
    GP0PAR = 0x0f; //01110
    GP0DAT = 0x10100000;

     

    regards,

    Mark

  • I have checked it for several weeks,

    In facts, the ADC is correct. the reason to make wrong data of ADC is that the DAC will not work when P0 is configured as analogue input. the DAC will not ouput linear voltage.

    Finally, when USE jlink, device works correctly after programming, but will not work correctly after reset again by power off and on.

    when use ULINK, device work incorrectly after programming, but it will work in debug mode, run or step by step. if the devcei is resetted again by poweroff/on, the devcei will not work correctly again.

  • hi, ramos,

    I have checked your code, it is wrong;

    ADC0CON = BIT8 + BIT7 // ADC0 input channel 6 in Single-Ended mode.
    + BIT15; // Auxiliary-ADC Enabled

    You use ADC0 to read channel6, it is wrong. ADC0 can't be used to read channel6~9. you can see datasheet.

    if you set BIT8+BIT7, the channel is not channel6, it is channel Vref+ and Vref-.

    Data reading by ADC0 is not output of DAC, it is voltage of Vref+ and Vref-.

    So wave in your picture and data from UART are wrong.

    They are fake.

  • Hi,
    In this example, I am using 2 ADCs at the same time.

    ADC0 measures from ADC2/ADC5 by setting ADC0CON = BIT8 + BIT7. I realized the comment there is wrong but on my board, I am forcing  voltage to ADC2 that is why I am reading the correct value. See screen shot from the datasheet below



    In my setup, I did not connect the DAC output to ADC input. I think this is the reason why you're getting a bad measurement. The ADC is probably loading the DAC. Do you have other circuit connected to your DAC? Can you disconnect the DAC from ADC and any other connection and re-run your code? 

  • sorry, ADC0CON = BIT8 + BIT7 set channel 2, not Vref+ and Vref-. I miss one bit;

    The test result of romas really validate the dac don't work correctly.

    As you see, midscale of Vref=1.2V is 0.6V

    midscale of Ver=2.5 is 1.25V

    You can see, the voltage 1.0v is hard to explain.

    romas said, it is little higher than 0.9V when he set DATDAT = 0xc000000.

    But if device works correctly, the output is very precise, error will not be so large.

    I compute here:

    when DATDAT = 0xc000000

    DAC output will be 0.9 when Vref = 1.2

    DAC output will be 1.85 when Vref = 2.5.

    In fact, if you want to output 1.0V, the devider should not be an integer because of prime number.

    I belive there is something wrong, perhaps romas can check it again

     

  • I just connect ADC4 and DAC together, and there is no other components.

    The spike you said generate because DAC output wrong leven when GP0CON1 = 0x0 change to GP0CON1 = 0x1. 

    with the same DACDAT the DAC will generate different voltage.

    You said you seen correct output, but why will not you to swap GP0CON1 = 0x0 and GP0CON1 = 0x1?

    It is easy to validate. I have give you good code, it is very easy to do this.

    I don't know why you insiste test code like that.

    In your code, it is very hard to identify what is relation between ADC1 ADC0, and Vref, and 0.6, 0.9, 1.0.

    All are in chaos.

  • The sps is 1k, from the code, bSendResultToUART = 1 always, it is not been cleared.

    so, when the DelayMs finish, the UART will report at once.

    from the code, you will find ADC1 should be constant, if  DACDAT = 0x0000000, ADC1 should be 0V, if DACDAT = 0x8000000; ADC1 should be 0.6V, constant, not swinging from 0 to 0.6V

    This is because ulADC1Result will be overwritten when DelayMs();

    another thing is:

    The result is 0.59V, if the ADC1 is used to sample DAC ouput, the error will not be so large, 0.59 give a error over/around 1%. It is not possible.

  • DACDAT = 0x8000000;
    DelayMs(10);

    sprintf ( (char*)szTemp, "ADC0 Result: %f\r",ulADC0Result*lsb10r9/1000000000 );

    this is because the ulADC0Result is used for the first report, and ulADC0Result  is used for the second report.

    So any value of ADC0 or ADC1 will be constant ( not considering noise), they will not swing.

    And you will find adc0 is about 1.0V. the value is wrong.

  • this is because the ulADC0Result is used for the first report, and ulADC1Result  is used for the second report.

  • Hi, 
    Please note that measurement through ADC6 to 9 inputs is only possible GP0CON1 = 0x1. I have checked switching between 0 and 1 value and I can still get correct measurement as long as GP0CON1 = 0x1 when doing the ADC measurement from ADC8 input. 

  • Hi,

    Please let me clarify the setup for my test:

    1. The board I used is the EVAL-ADUC7061MKZ so I can only download via UART downloader

    2. The example code that I provided configures the Primary and Auxiliary ADCs to use ADC2 and ADC8 as inputs respectively. I am using an external voltage source as an input to ADCs. No ADC is connected to any DAC, this is the reason why my result is showing a constant value even when DAC value is change. If I change the value in the voltage source then thats the time that the ADC result will change. 

    3. The DAC is configured to output zeroscale (0V) and midscale (0.6V) in a given time interval using VRef = 1.2V

    In conclusion, all the blocks are working fine even with P0 configured as an analog input. ADC8 is shared with P0.2 for ADUC7061 part and the DAC is still working as expected no spikes as reported in the original thread. 

    I will advise you to get the EVAL-ADUC7061MKZ and do your tests with this board. I am also open to reviewing your schematic and layout to see if there's anything that is causing the issue on your side. 

    regards,

    Mark

  • In your code:

    this is because the ulADC0Result is used for the first report, and ulADC1Result  is used for the second report.

    So, value of ADC1 will not swing, value ADC0 will not swing too.

    I don't know why you wave is square wave?

    Ok, I don't care the wave.

    You will find Vadc1/Vadc0 is not equal to DACDAT1/DACDAT0.  DACDAT1 is the second and DACDAT0 is the fist setting of DACDAT.

    In fact, I consider that you use wrong logic code. The C code is wrong. You can analysis your code logic carefully.

Reply
  • In your code:

    this is because the ulADC0Result is used for the first report, and ulADC1Result  is used for the second report.

    So, value of ADC1 will not swing, value ADC0 will not swing too.

    I don't know why you wave is square wave?

    Ok, I don't care the wave.

    You will find Vadc1/Vadc0 is not equal to DACDAT1/DACDAT0.  DACDAT1 is the second and DACDAT0 is the fist setting of DACDAT.

    In fact, I consider that you use wrong logic code. The C code is wrong. You can analysis your code logic carefully.

Children
No Data