Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC812: Status of the port on power-up
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • -ADuC812: FAQ
    • How to remove DAC zero Code error
    • ADUC812: Battery lifetime
    • ADuC812: Dealing with the interface I2C
    • Value of sample rate more higher that 200Ks are dangerous then customer never must use this value ?
    • ADuC812: enter serial download mode
    • ADuC812: Failure in restarting
    • ADUC812: Failure to Reset/Download
    • ADuC812: Flash reliability
    • ADuC812: glitches on the reset line
    • ADuC812: How to program external code space
    • ADuC812: latch-up
    • ADuC812: Measure ambient temperature
    • ADuC812: On Chip temperature sensor
    • ADuC812: Power down mode and choice of C compilers
    • ADuC812: Problems downloading to FLASH
    • ADuC812: PSEN pin
    • ADuC812: Reseting failure when downloading user program with WSD
    • ADuC812: serial interface
    • ADuC812: Status of the port on power-up
    • How do I migrate from ADuC812 to ADuC831 or ADu832?
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC812: Status of the port on power-up

Q 

- I use AD812 and wonder must I set the port 2 and 3 to  input/output n SFR or
does it do that automaticly?

 

A 

Some information of the status of ports 0, 1, 2 and 3 on power up. Where the
ADuC812 deviates from the "standard" 8051, I will explain the standard
situation and the ADuC812 situation.

Port 0
In the standard 8051 microcontroller, port 0 is either a bidirectional I/O port
or a multiplexed data/address port for accessing external memory. This is also
the case for the ADuC812. As shown on the datasheet (p 18), the P0 SFR (addr
80h) powers up as all "1"s (FFh), i.e. configured as a digital input. In the
standard 8051 implementation, when port 1 is configured as an input it is an
open drain circuit with the pull-down FET turned off and with no pull-up FET.
This is also the case for the ADuC812 and so port 1 will power up as a high
impedance input with no internal pull up.

Port 1
Port 1 on the ADuC812 differs from the standard 8051 implementation.
In the standard AD8051 implementation, port 1 can be configured as either a
digital input of a digital output (writing a 1 to the port pin latch configures
the pin as an input, writing a 0 to the port pin latch configures the part as
an output).
In the ADuC812, writing a 1 to the SFR configures port1 as an analog
input.Writing a 0 to the SFR configures the port as a digital input. The
default power up condition for the Port 1 register is all "1"s (note the
datasheet on page 18 is contradictory as it gives the default Port 1 SFR
contents as all "0"s (incorrectly) but the hex value is correctly given as FFh.)
Therefore the ADuC812 port 1 powers up with port 1 as 8 analog inputs. The
input mulitplexer connects P1.0 (pin 1) to the input of the ADC, which will
look approximately like a 10k resistance to ground. The remaining pins of port
1 are high impedance inputs.

Port 2 and Port 3
Ports 2 and 3 on the ADuC812 are similar to the standard 8051 implementation.
They can be configured as inputs or outputs but also have secondary functions
associated with them. On power up, ports 2 and 3 are configured as inputs by
default and have an internal pull up resistor, which is capable of sourcing up
to 80uA of current e.g. if the input is connected to ground.

Tags: aduc8xx aduc812 aduc8x