Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents How to remove DAC zero Code error
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • -ADuC812: FAQ
    • How to remove DAC zero Code error
    • ADUC812: Battery lifetime
    • ADuC812: Dealing with the interface I2C
    • Value of sample rate more higher that 200Ks are dangerous then customer never must use this value ?
    • ADuC812: enter serial download mode
    • ADuC812: Failure in restarting
    • ADUC812: Failure to Reset/Download
    • ADuC812: Flash reliability
    • ADuC812: glitches on the reset line
    • ADuC812: How to program external code space
    • ADuC812: latch-up
    • ADuC812: Measure ambient temperature
    • ADuC812: On Chip temperature sensor
    • ADuC812: Power down mode and choice of C compilers
    • ADuC812: Problems downloading to FLASH
    • ADuC812: PSEN pin
    • ADuC812: Reseting failure when downloading user program with WSD
    • ADuC812: serial interface
    • ADuC812: Status of the port on power-up
    • How do I migrate from ADuC812 to ADuC831 or ADu832?
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

How to remove DAC zero Code error

Q 

The offset of the on-board DAC of the ADUC8XX is 2% (5mV) in the range of 2.5V.
This causes a problem at the customer because they have to set the DAC out to
0-Volts.  The FS is not very important. Do you know how they can set the DAC
out to ZERO ?

 

A 

It will not be possible to get zero volts out of the DAC. The DAC has an on
offset of +/-50mV max. If the offset is  positive, the output voltage for the
zero code will be roughly equal to the offset voltage (with allowances made for
the headroom of the output amplifier).  If the offset is negative, the output
amplifier will saturate to near zero for the zero code. There will be a
"dead-band" around zero where the first few codes after zero will not produce
any response at the output. The output voltage will remain at zero for the
first few codes and then rise when the input code is equivalent to the offset
voltage.

There is no way to determine whether offset will be positive or negative.

If the customer requires a bipolar, true zero output, he can level shift the
output using an opamp circuit. The enclosed circuit will convert the 0 to 2.5V
output from the DAC to a +/-2.5V signal. You can then use software to calibrate
out the offset error. Since you only need 0 to 2.5V output, you will lose one
bit of resolution but I would not expect this to be a problem as the relative
accuracy of the DAC is only +/-3LSB anyway.

Tags: aduc8xx aduc812 aduc8x