Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC812: On Chip temperature sensor
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • -ADuC812: FAQ
    • How to remove DAC zero Code error
    • ADUC812: Battery lifetime
    • ADuC812: Dealing with the interface I2C
    • Value of sample rate more higher that 200Ks are dangerous then customer never must use this value ?
    • ADuC812: enter serial download mode
    • ADuC812: Failure in restarting
    • ADUC812: Failure to Reset/Download
    • ADuC812: Flash reliability
    • ADuC812: glitches on the reset line
    • ADuC812: How to program external code space
    • ADuC812: latch-up
    • ADuC812: Measure ambient temperature
    • ADuC812: On Chip temperature sensor
    • ADuC812: Power down mode and choice of C compilers
    • ADuC812: Problems downloading to FLASH
    • ADuC812: PSEN pin
    • ADuC812: Reseting failure when downloading user program with WSD
    • ADuC812: serial interface
    • ADuC812: Status of the port on power-up
    • How do I migrate from ADuC812 to ADuC831 or ADu832?
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC812: On Chip temperature sensor

Q 

I am doing development with the ADuC812.
Where can I find more detail information about the
"On-Chip-temperature-sensor"?
In the moment I have the "Preliminary Technical Data Sheet" - date of
issue
Mar./99. In that
paper I can only find  a small item on page -12- about that.

 

A 

You should refer to the REV.0 datasheet for the ADuC812 which is available on
our website:
www.analog.com/microconverter

The temperature sensor is inherently very linear (to about +/-2deg) but it is
not trimmed for absolute accuracy. We do not test the accuracy of the temp
sensor and therefore do not provide guaranteed specs. Typically the output of
the temp sensor is 650mV at room temperature with a tempco of -3.5mV/degC. To
make accurate absolute temperature measurements, you need to perform a two
point calibration and store the offset and gain co-efficients. Many designers
are using the temp sensor to determine when the ambient temperature has changed
"significantly" and using this to compensate a sensor for temperature drift.

Tags: aduc8xx aduc812 aduc8x