Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC812: serial interface
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • -ADuC812: FAQ
    • How to remove DAC zero Code error
    • ADUC812: Battery lifetime
    • ADuC812: Dealing with the interface I2C
    • Value of sample rate more higher that 200Ks are dangerous then customer never must use this value ?
    • ADuC812: enter serial download mode
    • ADuC812: Failure in restarting
    • ADUC812: Failure to Reset/Download
    • ADuC812: Flash reliability
    • ADuC812: glitches on the reset line
    • ADuC812: How to program external code space
    • ADuC812: latch-up
    • ADuC812: Measure ambient temperature
    • ADuC812: On Chip temperature sensor
    • ADuC812: Power down mode and choice of C compilers
    • ADuC812: Problems downloading to FLASH
    • ADuC812: PSEN pin
    • ADuC812: Reseting failure when downloading user program with WSD
    • ADuC812: serial interface
    • ADuC812: Status of the port on power-up
    • How do I migrate from ADuC812 to ADuC831 or ADu832?
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC812: serial interface

Q 

I would like to use the multiprocessor feature of the serial interface of the
ADuC812, in which bit 9 causes an serial interrupt if set. Unfortunately I
can't get this feature working, so I wonder if there is a software error or if
this feature is missing in the ADuC812. Here is my code:

$MOD812                         ; use ADuC812 predefined symbols

CSEG

ORG  0000h
  LJMP    START
ORG  0023h
  LJMP    SERIAL_INT
       
ORG  0030h

START:  
  MOV     SCON,#11110000B ; Mode 3, 9 bit, receive enable
  MOV     TMOD,#20H       ; timer 0 no function
                          ; timer 1 mode 2
  MOV     PCON,#00H       ; set SMOD
  MOV     TH1,#100H-3     ; reload 3 = 11.0592MHz/12/16/2/9600 bd
  SETB    TR1   ; start timer
  SETB    ES    ; enable serial interrupt
  CLR     PS    ; serial interrupt low priority
  SETB    EA    ; general interrupt enable
       
LOOP:
  JMP     LOOP  ; repeat indefinately

SERIAL_INT:
  PUSH    PSW
  PUSH    ACC
  MOV     A,SBUF          ; get character
  CPL     P3.4            ; toggle LED
  CLR     RI              ; clear receive flag
  POP     ACC
  POP     PSW
  RETI
END

This program should run directly on the evaluation board, it toggles the LED
each time it gets a serial interrupt. Now I send data from my PC with and
without bit9 set, but both cause the interrupt. I ensure the PC program is
correct by looking at the signals with a digital scope.


P.S.: Can I run the ADuC812 with an 11,0592MHZ quartz at 115200 baud?

 

A 

This is a known bug on the ADuC812 and covered in item 3 of the current Errata
sheet (REV E). The full errata sheet is available on our website:
www.analog.com/microconverter

3. UART FUNCTION - MULTIPROCESSOR COMMUNICATIONS MODE :
Background: UART Modes 2 and 3 (programmed via SCON) have a special provision
for multiprocessor communications. In these modes, nine data bits are
received and the ninth bit goes into RB8. In this mode the port can be
programmed so that when the stop bit is received, the serial port interrupt
is activated only if RB8(SCON) = 1. This feature is enabled by setting the
SM2 bit in SCON.
Issue: With SM2 set, the serial port interrupt is set each time a stop bit is
received, regardless of the state of the RB8 bit.
Work-Around : Implement a software polling scheme in the Serial Port ISR so
that the
state of the RB8 bit is checked on entering the ISR. If RB8 is ‘0’ then a
‘RETI’ is executed to exit the ISR immediately, and only if RB8 is set will
the ISR function be executed.
Related Issues : None.

Tags: aduc8xx aduc812 aduc8x