Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC812: Flash reliability
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • -ADuC812: FAQ
    • How to remove DAC zero Code error
    • ADUC812: Battery lifetime
    • ADuC812: Dealing with the interface I2C
    • Value of sample rate more higher that 200Ks are dangerous then customer never must use this value ?
    • ADuC812: enter serial download mode
    • ADuC812: Failure in restarting
    • ADUC812: Failure to Reset/Download
    • ADuC812: Flash reliability
    • ADuC812: glitches on the reset line
    • ADuC812: How to program external code space
    • ADuC812: latch-up
    • ADuC812: Measure ambient temperature
    • ADuC812: On Chip temperature sensor
    • ADuC812: Power down mode and choice of C compilers
    • ADuC812: Problems downloading to FLASH
    • ADuC812: PSEN pin
    • ADuC812: Reseting failure when downloading user program with WSD
    • ADuC812: serial interface
    • ADuC812: Status of the port on power-up
    • How do I migrate from ADuC812 to ADuC831 or ADu832?
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC812: Flash reliability

Q 

One customer is asking about the flash spec of the ADuC812. The datasheets
tells, that the data in the flash will remain for 10 years, but this spec is
for 5V supply!

What about this spec under 3.3V operation? Also 10 years?

 

A 

We did not have the available 3V data for Flash/EE characteristics when we
released the ADuC812 and therefore we only included 5V maximum specifications
on the datasheet and typical specification for endurance at 3V supplies.

I should also draw your attention to the fact that we do have an errata on 3V
programming which is included in our current errata sheet, errata #7. This
means that some small percentage of devices may fail to program correctly
(~1%), I should also add however that once the devices do program at 3V they
are guaranteed as per our reliability specifications.

Recently, we have been produced a new mask set for this part, we were limited
in the modifications we could make as the 'new' mask only modified the metal
layer. However even with this limited edit we now have a new revision of the
ADuC812 which will program down to 2.7V from 0ºC to +85ºC, the programming
errata will remain for temperatures below 0ºC.

At this time, the new revision of silicon is under going comprehensive
qualification of the FLASH memory for retention and endurance. This new
material should come on line through the Summer timeframe.

With respect to 3V reliability, this silicon is now also qualified for 3V
operation and the 5V specifications for retention and endurance also now apply
to 3V operation. Finally I should also draw your attention to the fact that our
more recent MicroConverter releases ADuC816 and ADuC824 have improved
reliability specifications 100K endurance and 100 year retention, these parts
run on the same Flash process as the ADuC812 and therefore we will be in a
position to step up to these revised figures once the ADuC812 completes a
further internal qualification cycle.

Tags: aduc8xx aduc812 aduc8x