Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents Value of sample rate more higher that 200Ks are dangerous then customer never must use this value ?
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • -ADuC812: FAQ
    • How to remove DAC zero Code error
    • ADUC812: Battery lifetime
    • ADuC812: Dealing with the interface I2C
    • Value of sample rate more higher that 200Ks are dangerous then customer never must use this value ?
    • ADuC812: enter serial download mode
    • ADuC812: Failure in restarting
    • ADUC812: Failure to Reset/Download
    • ADuC812: Flash reliability
    • ADuC812: glitches on the reset line
    • ADuC812: How to program external code space
    • ADuC812: latch-up
    • ADuC812: Measure ambient temperature
    • ADuC812: On Chip temperature sensor
    • ADuC812: Power down mode and choice of C compilers
    • ADuC812: Problems downloading to FLASH
    • ADuC812: PSEN pin
    • ADuC812: Reseting failure when downloading user program with WSD
    • ADuC812: serial interface
    • ADuC812: Status of the port on power-up
    • How do I migrate from ADuC812 to ADuC831 or ADu832?
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

Value of sample rate more higher that 200Ks are dangerous then customer never must use this value ?

Q 

In A/D timing for ADuC812 normaly I use low frequency of sample ( 50Khz and
lower) In DS AD declare that Frequency of A/D is MCLK / CK1,CK0 bit  plus 
AQ1,AQ0  table value
If I use 16Mhz clock I have a T of 1/16e6  = 62.5nS

One A/D conversione need of 16 ADC clk;
If I selecting CK1 and CK0 to zero MCLK divider is 1 .
Than for A/D conversion timing is (62.5ns  x 16 ) plus AQ1, AQ0 table value
If I select AQ1 = 0 and AQ0 = 1  my final value is :
(62.5ns x 16 ) + (62.5ns x 2)  = 1uS + 125ns = 1,125nS
This is value for 888Ksps!!
A/D on chip for AduC812 have a target for 200KspS or 5uS
My question is : Value of sample rate more higher that 200Ks are dangerus then
customer never must use this value ?

A 

The ADuC812’s successive approximation ADC is driven by a divided down version
of the master clock. To ensure adequate ADC operation, this ADC clock must be
between 400KHz and 4MHz., and optimum performance is obtained with ADC clock
between 400KHz and 3MHz. Frequencies within this range can easily be achieved
with master clock frequencies from 400KHz to well above 16MHz with the four ADC
clock divide ratios to choose from. For example, with a 12MHz master clock, set
the ADC clock divide ratio to 4 (i.e. ADCCLK = MCLK / 4 = 3MHz) by setting the
appropriate bits in ADCCON1 (ADCCON1.5=1, ADCCON1.4=0).

There is no mechanism to prevent the user selecting an ADC conversion rate
higher than the recommended 200kHz. Selecting a conversion rate higher than
200kHz will not damage the part but the performance will be severly degraded.

Also note that at fast ADC conversion rates the micro core will not have much
time between serving ADC interuppts to do any calculations. Generally users
will make use of DMA mode when using fast conversion rates.

Tags: aduc8xx aduc812 aduc8x