Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC812: Problems downloading to FLASH
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • -ADuC812: FAQ
    • How to remove DAC zero Code error
    • ADUC812: Battery lifetime
    • ADuC812: Dealing with the interface I2C
    • Value of sample rate more higher that 200Ks are dangerous then customer never must use this value ?
    • ADuC812: enter serial download mode
    • ADuC812: Failure in restarting
    • ADUC812: Failure to Reset/Download
    • ADuC812: Flash reliability
    • ADuC812: glitches on the reset line
    • ADuC812: How to program external code space
    • ADuC812: latch-up
    • ADuC812: Measure ambient temperature
    • ADuC812: On Chip temperature sensor
    • ADuC812: Power down mode and choice of C compilers
    • ADuC812: Problems downloading to FLASH
    • ADuC812: PSEN pin
    • ADuC812: Reseting failure when downloading user program with WSD
    • ADuC812: serial interface
    • ADuC812: Status of the port on power-up
    • How do I migrate from ADuC812 to ADuC831 or ADu832?
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC812: Problems downloading to FLASH

Q 

We have a customer trying to use the EVAL BD for the ADUC812 - he has had this
for some time but is now reporting a 'download limit' preventing the system
from working - even s/w written some time ago that used to work is no longer
functioning.

Is there a 'timeout' feature on the eval kit preventing it being used after 12
months or so?
Or can you offer any advice as to anything that has changed which would now
prevent the correct opporation of the product (perhaps a device modification
etc ? ).

 

A 

There is no deliberate "download limit" whatsoever on the ADuC812 or its
evaluation board.

Reading between the lines, the customer seems to be unable to download code to
the on board FLASH memory.
There are two likely causes to the problem of being unable to re-program the
FLASH. Either your software has written to a FLASH location higher than 159Hor 
a spurious RESET signal has caused the ADuC812 to begin executing with a supply
less than 2V. let's look at both these possibilities in more detail.

-Code downloaded fine a few times, but now always "fails to reset the
target"....If the last program to successfully go onto the chip contains any
commands to program the 640 byte Flash/EE data space, then it's possible that a
simple programming error caused a write to page 160 resulting in the security
bits getting set and locking the chip up for good. There's no way to recover
other than replacing the chip. Code must be written carefully to ensure that
page 160 of data Flash/EE space never gets programmed. See errata #7 (errata
revs E & D) for details.

-Check the reset signal on your board. Are there any glitches on it? Look at
the reference on the mis-behaving parts, is it exactly at 2.5V? If the micro is
released from reset while DVDD is below 2V, the micro will still execute code
without trouble. However, if you try to write to the FLASH while the power
supply is low, the on -chip charge pumps cannot generate the required
programming voltages. Exactly what happens in these circumstances is
indeterminate but one possibility is that the calibration co-efficients are
erased and this would cause the reference to jump to 2.8V, the ADC would not be
accurate and it would also be possible to lock the code space on the part such
that it cannot be reprogrammed. So check your RESET line, and, if necessary 
replace your reset generator with one that follows VDD during power up and then
releases RESET a few 100ms after DVDD is fully up. The ADM1817, ADM1813, ADM809
would be ideal here. If you have erased the cal co-efficients, the part must be
replaced, there is no way to reload these co-efficients once they are lost.

Tags: aduc8xx aduc812 aduc8x