Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Unpacking IEC 61508: Low Complexity versus Type A Made Simple

    IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...

     

    Taming the AI Power Storm: Part 2 of 3

    Let’s peel back the curtain on how Analog Devices (ADI) is leading the charge, crafting power solutions that not only keep up with AI’s appetite but redefine...

    Latest Blogs

    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
    • ​​Where Errors Lurk in the GMSL Signal Chain​
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
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC814: Digital I/O configuration
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • -ADUC814: FAQ
    • For ADUC814, what is the minimum time and level of the reset impulse I need to ensure a CPU reset? VDD is 4V.
    • ADuC814: Digital I/O configuration
    • ADUC814: Internal Temperature sensor specifications
    • ADuC814: Temperature sensor
    • EVAL-ADUC841 A4 Schematics
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC814: Digital I/O configuration

Q 

Can I program Port 1 and 3 as input or output, ie is it to send logic 1 or
logic 0 via port 1 and 3? In the document, it says, whenever you write 0, it
becomes input. It also says P1.2-P1.7 cannot be configured as digital output.
But it should drive base of a transistor connected to P1.2-P1.7 if I write 1 to
P1.2-P1.7.

 

A 

Each of the pins of Port 3 can be an input or an output. If you write a 0 to
the bit location in the P3 register, the pin outputs a digital low. If you
write a 1 to the bit location, the pin is pulled high by an internal pull-up
and in addition, a strong pull up is active briefly, to speed up the 0-1
transition.

Pins P1.0 and P1.1 fucntion like the port 3 pins. All the other port 1 pins can
only be digital inputs or analog inputs (to the ADC). To get them to be digital
inputs, you need to write a 0 to the bit location in the P1 register. To get
them to be ADC input pins, write a 1 to the port bit and configure ADCCON2.3~0
to select the required channel.

There is no output circuitry on P1.2~P1.7 so thay CANNOT even be used to drive
transistor bases, as you describe.

Tags: aduc8xx aduc814 aduc8x
  • Share
  • History
  • More