Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADUC834: Can I use analog inputs on Port 1 pins for digital I/0?
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • -ADUC834: FAQ
    • The ADuC834 has separate pins for analog and digital power supplies. Can I run from a split supply, for example a 3.3V DVDD and a 5V AVDD?
    • ADUC834: Can I convert a single-ended input voltage by grounding one of primary ADC diff inputs?
    • ADUC834: Can I use analog inputs on Port 1 pins for digital I/0?
    • ADUC834: Do I need external reset generator?
    • ADUC834: Does changing the PLL divider value via the CD bits in PLLCON affect the baud rate?
    • ADUC834: Driving LEDs directly from digital outputs, what pins should I use?
    • ADUC834: How do I configure the UART serial port at 9600/115200 baud?
    • ADUC834: How do I use the on-chip temperature sensor feature of the ADuC834?
    • ADUC834: I am changing ranges and I am seeing much more than 2uV gain mis-match. Why?
    • ADUC834: I want to initiate the serial downloader through the SPI port, how can I do this?
    • ADUC834: Impact of fast logic edges on analog performance
    • ADuC834: Interfacing the ADuC834 to a RTD
    • ADUC834: Is it possible to accidently write to security bits and prevent part entering download mode?
    • ADUC834: Is it possible to switch OFF the internal buffer of primary ADC?
    • ADUC834: Minimum and maximum external voltage references allowed by the ADuC834.
    • ADUC834: Overwriting the ADC factory calibration coefficients
    • ADuC834: pinout decriptions missing for CSP pins 28and 29
    • ADUC834: Should I use the internal voltage reference or an external voltage reference?
    • ADUC834: The reference input is differential. Can I use a single ended reference?
    • ADUC834: Use of PSEN pin on Microcontroller v 8051
    • ADuC834: Values of the internal pull up resistor
    • ADUC834: What are the implications of having unbuffered differential reference inputs?
    • ADUC834: What baud rates can be achieved?
    • ADUC834: What external clocks can be used? Can the PLL be bypassed?
    • ADUC834: What is lowest power consumption configuration for 10 hour sample conversion intervals?
    • ADUC834: What is the minimum time (or ADC cycles) to get a reading if the input is a step?
    • ADUC834: What's the difference between the INL spec and the noise spec on the ADC?
    • ADUC834: Why does ADC effective resolution depend on range and update rate
    • ADUC834: Why is there a different result when using internal voltage ref compared to external 2.5V ref?
    • Why does it take the ADuC834 so long to power on?
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADUC834: Can I use analog inputs on Port 1 pins for digital I/0?

Revision Creation Date Revision Author
Current Revision 29 Oct 2021 2:05 PM GenevaC
Revision #2 7 Jan 2021 4:50 PM EZAdministrator
Revision #1 4 Jun 2018 12:53 PM analog-archivist
  • Compare Versions View current version