This webinar will introduce remote-controlled edge nodes and how they promise to simplify the automotive network architecture and expedite the integration...
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
      1. Quote of the week: "Knowledge is knowing a tomato is a fruit. Wisdom is not putting it in a fruit salad" - unknown Sources: commons.wikimedia...

    View All

    What's Brewing

      Quiz! Why a Hybrid Approach Works Blog and Test Your Knowledge

      Quiz! Understand ISO 26262 Compliance Test your knowledge with our quick quiz , based on the blog " Safety in Layers: Why a Hybrid Approach Works ...
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
    The Limitation of Heat Dissipation IO-Link is used across many branches of factory automation, and in these applications, areas of the factory floor...

     

    GMSL Debugging: Getting a Lock

    Imagine a scenario where you have a brand-new board design or are excited to try out some evaluation kits only to find out that the two devices can’t talk...
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
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Microcontrollers
8052 Core Products
Documents ADUC834: What baud rates can be achieved?
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • More
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • -ADUC834: FAQ
    • The ADuC834 has separate pins for analog and digital power supplies. Can I run from a split supply, for example a 3.3V DVDD and a 5V AVDD?
    • ADUC834: Can I convert a single-ended input voltage by grounding one of primary ADC diff inputs?
    • ADUC834: Can I use analog inputs on Port 1 pins for digital I/0?
    • ADUC834: Do I need external reset generator?
    • ADUC834: Does changing the PLL divider value via the CD bits in PLLCON affect the baud rate?
    • ADUC834: Driving LEDs directly from digital outputs, what pins should I use?
    • ADUC834: How do I configure the UART serial port at 9600/115200 baud?
    • ADUC834: How do I use the on-chip temperature sensor feature of the ADuC834?
    • ADUC834: I am changing ranges and I am seeing much more than 2uV gain mis-match. Why?
    • ADUC834: I want to initiate the serial downloader through the SPI port, how can I do this?
    • ADUC834: Impact of fast logic edges on analog performance
    • ADuC834: Interfacing the ADuC834 to a RTD
    • ADUC834: Is it possible to accidently write to security bits and prevent part entering download mode?
    • ADUC834: Is it possible to switch OFF the internal buffer of primary ADC?
    • ADUC834: Minimum and maximum external voltage references allowed by the ADuC834.
    • ADUC834: Overwriting the ADC factory calibration coefficients
    • ADuC834: pinout decriptions missing for CSP pins 28and 29
    • ADUC834: Should I use the internal voltage reference or an external voltage reference?
    • ADUC834: The reference input is differential. Can I use a single ended reference?
    • ADUC834: Use of PSEN pin on Microcontroller v 8051
    • ADuC834: Values of the internal pull up resistor
    • ADUC834: What are the implications of having unbuffered differential reference inputs?
    • ADUC834: What baud rates can be achieved?
    • ADUC834: What external clocks can be used? Can the PLL be bypassed?
    • ADUC834: What is lowest power consumption configuration for 10 hour sample conversion intervals?
    • ADUC834: What is the minimum time (or ADC cycles) to get a reading if the input is a step?
    • ADUC834: What's the difference between the INL spec and the noise spec on the ADC?
    • ADUC834: Why does ADC effective resolution depend on range and update rate
    • ADUC834: Why is there a different result when using internal voltage ref compared to external 2.5V ref?
    • Why does it take the ADuC834 so long to power on?
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADUC834: What baud rates can be achieved?

Revision Creation Date Revision Author
Current Revision 29 Oct 2021 2:21 PM GenevaCooper
Revision #2 7 Jan 2021 4:50 PM EZAdministrator
Revision #1 4 Jun 2018 12:53 PM analog-archivist
  • Compare Versions View current version