Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADUC834: What are the implications of having unbuffered differential reference inputs?
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • -ADUC834: FAQ
    • The ADuC834 has separate pins for analog and digital power supplies. Can I run from a split supply, for example a 3.3V DVDD and a 5V AVDD?
    • ADUC834: Can I convert a single-ended input voltage by grounding one of primary ADC diff inputs?
    • ADUC834: Can I use analog inputs on Port 1 pins for digital I/0?
    • ADUC834: Do I need external reset generator?
    • ADUC834: Does changing the PLL divider value via the CD bits in PLLCON affect the baud rate?
    • ADUC834: Driving LEDs directly from digital outputs, what pins should I use?
    • ADUC834: How do I configure the UART serial port at 9600/115200 baud?
    • ADUC834: How do I use the on-chip temperature sensor feature of the ADuC834?
    • ADUC834: I am changing ranges and I am seeing much more than 2uV gain mis-match. Why?
    • ADUC834: I want to initiate the serial downloader through the SPI port, how can I do this?
    • ADUC834: Impact of fast logic edges on analog performance
    • ADuC834: Interfacing the ADuC834 to a RTD
    • ADUC834: Is it possible to accidently write to security bits and prevent part entering download mode?
    • ADUC834: Is it possible to switch OFF the internal buffer of primary ADC?
    • ADUC834: Minimum and maximum external voltage references allowed by the ADuC834.
    • ADUC834: Overwriting the ADC factory calibration coefficients
    • ADuC834: pinout decriptions missing for CSP pins 28and 29
    • ADUC834: Should I use the internal voltage reference or an external voltage reference?
    • ADUC834: The reference input is differential. Can I use a single ended reference?
    • ADUC834: Use of PSEN pin on Microcontroller v 8051
    • ADuC834: Values of the internal pull up resistor
    • ADUC834: What are the implications of having unbuffered differential reference inputs?
    • ADUC834: What baud rates can be achieved?
    • ADUC834: What external clocks can be used? Can the PLL be bypassed?
    • ADUC834: What is lowest power consumption configuration for 10 hour sample conversion intervals?
    • ADUC834: What is the minimum time (or ADC cycles) to get a reading if the input is a step?
    • ADUC834: What's the difference between the INL spec and the noise spec on the ADC?
    • ADUC834: Why does ADC effective resolution depend on range and update rate
    • ADUC834: Why is there a different result when using internal voltage ref compared to external 2.5V ref?
    • Why does it take the ADuC834 so long to power on?
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADUC834: What are the implications of having unbuffered differential reference inputs?

Q 

What are the implications of having unbuffered differential reference inputs?

 

A 

The unbuffered reference input provides a high impedance, dynamic load. Because
the input
impedance of each reference input is dynamic, resistor/capacitor combinations
on these inputs can
cause dc gain errors depending on the output impedance of the source that is
driving the reference
inputs. Reference voltage sources, like those recommended (AD780) will
typically have low
output impedances and therefore decoupling capacitors on the REFIN(+) and
REFIN(-) inputs
would be recommended. Driving the reference input voltage across an external
resistor, as in many
ratiometric configurations, will mean that the reference input sees a
significant external source
impedance. External decoupling on the REFIN(+) and REFIN(-) pins would not be
recommended
in this type of circuit configuration.

Tags: aduc8xx aduc8x aduc834