This webinar will introduce remote-controlled edge nodes and how they promise to simplify the automotive network architecture and expedite the integration...
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
      1. Quote of the week: "Knowledge is knowing a tomato is a fruit. Wisdom is not putting it in a fruit salad" - unknown Sources: commons.wikimedia...

    View All

    What's Brewing

      Quiz! Why a Hybrid Approach Works Blog and Test Your Knowledge

      Quiz! Understand ISO 26262 Compliance Test your knowledge with our quick quiz , based on the blog " Safety in Layers: Why a Hybrid Approach Works ...
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
    The Limitation of Heat Dissipation IO-Link is used across many branches of factory automation, and in these applications, areas of the factory floor...

     

    GMSL Debugging: Getting a Lock

    Imagine a scenario where you have a brand-new board design or are excited to try out some evaluation kits only to find out that the two devices can’t talk...
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
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Microcontrollers
8052 Core Products
Documents ADUC: Addressing up to 16Mbytes of external data memory
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • More
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • -ADuC842: FAQ
    • Using ADuC842 as master on a multimaster I2C bus
    • Program halts or operates incorrectly with ADuC842 at 16.78MHz
    • ADUC842 port 3 internal pull-up electrical characteristics
    • -ADUC: Should I connect devices analog and digital ground pins to separate ground planes?
      • ADUC: Addressing up to 16Mbytes of external data memory
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADUC: Addressing up to 16Mbytes of external data memory

Q 

Can the ADuC microcontroller address up to 16Mbytes of external data memory. Is
so, how is it done?

 

A 

The Microcontroller can address up to 16Mbytes of external data memory. If
access to more
than 64 Kbytes of RAM is desired, a feature unique to the microcontroller
allows addressing up to
16 Mbytes of external RAM simply by adding an additional latch on the Port 2
address bus.
On a standard 8051 as with the Microcontrollerr Port 0 (P0) serves as a
multiplexed address/data
bus. It emits the low byte of the data pointer (DPL) as an address, which is
latched by a pulse of
ALE prior to data being placed on the bus by the microcontroller (write
operation) or the SRAM
(read operation). Port 2 (P2) provides the data pointer page byte (DPP) to be
latched by ALE,
followed by the data pointer high byte (DPH). If no latch is connected to P2,
DPP is ignored by the
SRAM, and the 8051 standard of 64kByte external data memory access is
maintained.
Tags: aduc8xx aduc8x aduc834