Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADUC834: Use of PSEN pin on Microcontroller v 8051
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • -ADUC834: FAQ
    • The ADuC834 has separate pins for analog and digital power supplies. Can I run from a split supply, for example a 3.3V DVDD and a 5V AVDD?
    • ADUC834: Can I convert a single-ended input voltage by grounding one of primary ADC diff inputs?
    • ADUC834: Can I use analog inputs on Port 1 pins for digital I/0?
    • ADUC834: Do I need external reset generator?
    • ADUC834: Does changing the PLL divider value via the CD bits in PLLCON affect the baud rate?
    • ADUC834: Driving LEDs directly from digital outputs, what pins should I use?
    • ADUC834: How do I configure the UART serial port at 9600/115200 baud?
    • ADUC834: How do I use the on-chip temperature sensor feature of the ADuC834?
    • ADUC834: I am changing ranges and I am seeing much more than 2uV gain mis-match. Why?
    • ADUC834: I want to initiate the serial downloader through the SPI port, how can I do this?
    • ADUC834: Impact of fast logic edges on analog performance
    • ADuC834: Interfacing the ADuC834 to a RTD
    • ADUC834: Is it possible to accidently write to security bits and prevent part entering download mode?
    • ADUC834: Is it possible to switch OFF the internal buffer of primary ADC?
    • ADUC834: Minimum and maximum external voltage references allowed by the ADuC834.
    • ADUC834: Overwriting the ADC factory calibration coefficients
    • ADuC834: pinout decriptions missing for CSP pins 28and 29
    • ADUC834: Should I use the internal voltage reference or an external voltage reference?
    • ADUC834: The reference input is differential. Can I use a single ended reference?
    • ADUC834: Use of PSEN pin on Microcontroller v 8051
    • ADuC834: Values of the internal pull up resistor
    • ADUC834: What are the implications of having unbuffered differential reference inputs?
    • ADUC834: What baud rates can be achieved?
    • ADUC834: What external clocks can be used? Can the PLL be bypassed?
    • ADUC834: What is lowest power consumption configuration for 10 hour sample conversion intervals?
    • ADUC834: What is the minimum time (or ADC cycles) to get a reading if the input is a step?
    • ADUC834: What's the difference between the INL spec and the noise spec on the ADC?
    • ADUC834: Why does ADC effective resolution depend on range and update rate
    • ADUC834: Why is there a different result when using internal voltage ref compared to external 2.5V ref?
    • Why does it take the ADuC834 so long to power on?
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADUC834: Use of PSEN pin on Microcontroller v 8051

Q 

The PSEN pin is always an output on an 8051. How then can it be used as an
input to enter serial
download mode? What pulldown resistor should be used to be sure to enter serial
download
mode? Is the standard functionality of the PSEN pin affected?

 

A 

On an 8051 the PSEN pin is always an output. It is used to access external code
memory. On the
Microcontroller the PSEN pin is used to access external code memory and is used
as an input to
determine whether to run user code or run the on chip serial downloader.
The PSEN pin is normally configured as an output. When the RESET pin is pulled
high, the
PSEN pin becomes a digital input and the voltage at the PSEN pin is sampled
every machine
cycle. Once the RESET pin is released (low) the last sampled logic level of the
PSEN pin is used
to decide whether to run from user code or whether to run the on chip serial
downloader.
To ensure that the PSEN pin is interpreted as a logic low it should be pulled
low through a 1k
resistor to ground. To ensure that the PSEN pin is interpreted as a logic high
it can be left float as
there is an internal pullup resistor.
Because the functionality of the PSEN pin on the ADUC8xx Microcontroller only
differs from that of an
8051 when RESET is pulled high (in this condition the PSEN pin on an 8051 is
useless) the
functionality of the PSEN pin on the ADUC8xx Microcontroller is unaffected by
its additional functionality.

Tags: aduc8xx aduc8x aduc834
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • ADuC812: PSEN pin
    GenevaC
    Q Can the PSEN pin be pulled low during the duration of the serial programming or are there any specific timing requirements re this line during serial programming? I am not using any external memory...
  • ADUC841 PSEN voltage level
    Oppie
    I have several ADuC841 devices that are on a common serial programming bus. This is used for field reprogramming of the device in a much larger system. A host processor port is asseting the psen line...
 
Related Content
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • ADuC812: PSEN pin
    GenevaC
    Q Can the PSEN pin be pulled low during the duration of the serial programming or are there any specific timing requirements re this line during serial programming? I am not using any external memory...
  • ADUC841 PSEN voltage level
    Oppie
    I have several ADuC841 devices that are on a common serial programming bus. This is used for field reprogramming of the device in a much larger system. A host processor port is asseting the psen line...