Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Evaluating Power Supplies with Different Compensation Settings

    Evaluating Power Supplies with Different Compensation Settings

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC834: Interfacing the ADuC834 to a RTD
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • -ADUC834: FAQ
    • The ADuC834 has separate pins for analog and digital power supplies. Can I run from a split supply, for example a 3.3V DVDD and a 5V AVDD?
    • ADUC834: Can I convert a single-ended input voltage by grounding one of primary ADC diff inputs?
    • ADUC834: Can I use analog inputs on Port 1 pins for digital I/0?
    • ADUC834: Do I need external reset generator?
    • ADUC834: Does changing the PLL divider value via the CD bits in PLLCON affect the baud rate?
    • ADUC834: Driving LEDs directly from digital outputs, what pins should I use?
    • ADUC834: How do I configure the UART serial port at 9600/115200 baud?
    • ADUC834: How do I use the on-chip temperature sensor feature of the ADuC834?
    • ADUC834: I am changing ranges and I am seeing much more than 2uV gain mis-match. Why?
    • ADUC834: I want to initiate the serial downloader through the SPI port, how can I do this?
    • ADUC834: Impact of fast logic edges on analog performance
    • ADuC834: Interfacing the ADuC834 to a RTD
    • ADUC834: Is it possible to accidently write to security bits and prevent part entering download mode?
    • ADUC834: Is it possible to switch OFF the internal buffer of primary ADC?
    • ADUC834: Minimum and maximum external voltage references allowed by the ADuC834.
    • ADUC834: Overwriting the ADC factory calibration coefficients
    • ADuC834: pinout decriptions missing for CSP pins 28and 29
    • ADUC834: Should I use the internal voltage reference or an external voltage reference?
    • ADUC834: The reference input is differential. Can I use a single ended reference?
    • ADUC834: Use of PSEN pin on Microcontroller v 8051
    • ADuC834: Values of the internal pull up resistor
    • ADUC834: What are the implications of having unbuffered differential reference inputs?
    • ADUC834: What baud rates can be achieved?
    • ADUC834: What external clocks can be used? Can the PLL be bypassed?
    • ADUC834: What is lowest power consumption configuration for 10 hour sample conversion intervals?
    • ADUC834: What is the minimum time (or ADC cycles) to get a reading if the input is a step?
    • ADUC834: What's the difference between the INL spec and the noise spec on the ADC?
    • ADUC834: Why does ADC effective resolution depend on range and update rate
    • ADUC834: Why is there a different result when using internal voltage ref compared to external 2.5V ref?
    • Why does it take the ADuC834 so long to power on?
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC834: Interfacing the ADuC834 to a RTD

Q 

I've got two questions:
1. Is there any performance difference between old RTD connection (in ADuC824
datasheet with ref resistor connected to EXC) and new RTD connection (in
ADuC834 datasheet with ref resistor connected to AGND)?
2. Can I connect two RTDs serially (4 way connection each) and measure their
resistance on AIN1-2 and AIN3-4? What would be suggested decoupling (if any)?

 

A 

There is no performance difference between the two implementations. The circuit
shown on the ADuC834 datasheet is advantageous as it uses one less resistor.

The key requirements are:
Maximize the full-scale voltage drop across the RTD to maximize resolution
Keep the total voltage drop across the sense resistors and RTD within the
voltage compliance range of the current source (VDD-0.6V)
And ensure you meet the input common mode requirements of the ADC input
(AGND+100mV to VDD-100mV).

Yes it is possible to use multiple RTDs with the same current source (in
series). Again, simply ensure you meet the voltage compliance range of the
current source and the input range of the ADC.

Decoupling requirements will depend on how harsh an environement the RTD are
placed in. If the RTDs are on the same board as the ADuC, not exposed to noise
and the ADuC power supply is well decoupled, you probably will not require any
decoupling capacitors on the analog inputs.

However, if the RTDs are located remotely via long cables in an electrically
harsh environment (lots of magnetic field and EMI) you will need to look at
adding capacitors to filter the spurious signals. 10nF would be a good starting
point but I suspect a little trial and error coupled with a reasonable estimate
of the likely interference / noise signals will provide the best solution.

Tags: aduc8xx aduc8x aduc834
  • Share
  • History
  • More