Q
I have found on your website the Quick Starts Kits for ADuC800 series, but in
the purchase list ADUC836 is not there. Can you suggest which type of kit I can
use?
A
There was never a development system for ADUC836. Instead we recommend you use
the development system for ADuC834.
ADuC834 v ADuC836:
834 has 2 ADCs, 24 bit ADC and 16 bit ADC
836 has 2 ADCs, both 16 bit
There is a note on the ADuC834 development system web page:
Development system for evaluation of the ADuC834, 24-Bit ADC + 16-Bit ADC +
12-Bit DAC + 62K-Byte Flash MCU. This development system is also recommanded
for evaluation of ADuC836, Dual 16-Bit ADC + 12-Bit DAC + 62K-Byte Flash MCU.