Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC84X. About ADuC84x external memory debug
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • -ADuC84x: FAQ
    • ADuC84x, tolerance of PLL output frequency
    • ADuC84X. About ADuC84x external memory debug
    • ADUC84x: What state are the port pins set to, when the device is using the factory installed bootloader?
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC84X. About ADuC84x external memory debug

Q 

As we know, ADuC84x can expand up to 16Bbyte XRAM by 24bit addressing. Can we
use Keil to debug the system when using external RAM? If yes, how do we
debug/observe the external data in Keil?

 

A 

Yes, keil can debug the full external SRAM memory.
We don’t have an evaluation board with external SRAMs on it but, it will work
if Port0/Port2/ALE/RD/WR pins are connected to external memory.
You just need to populate the target memory menu that you highlighted and set
up the external memory SFRs in user code.
When debugging, just open the memory window and scroll to the appropriate
address.

Tags: aduc8xx aduc8x aduc841
  • Share
  • History
  • More