Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADUC842 port 3 internal pull-up electrical characteristics
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • -ADuC842: FAQ
    • Using ADuC842 as master on a multimaster I2C bus
    • Program halts or operates incorrectly with ADuC842 at 16.78MHz
    • ADUC842 port 3 internal pull-up electrical characteristics
    • +ADUC: Should I connect devices analog and digital ground pins to separate ground planes?
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADUC842 port 3 internal pull-up electrical characteristics

Q 

I'm using an ADuC842 and I noticed that on the datasheet there are few and no
specific indications about the electrical characteristics of the internal
pull-up on port 3, can you provide more information?

 

A 

The port 3 pins have a finite and non-linear output impedance i.e. the voltage
will change according to how much current you draw.

We specify this in the following way (see page 5 of the datasheet, section on
digital outputs).

Voh output voltage high:
> 2.4V when Isource < 80uA and power supply >4.5V
> 4.0V when Isource < 20uA and power supply >4.5V
so basically, when you draw > 80uA from the part we can't guarantee that the
"high" voltage will stay above the 2.4V required to be a logic high in TTL.
This makes it a fairly weak output and shouldn't be used to drive anything that
needs significant current.

Port 3, Vol output voltage low:
< 0.4V when Isink < 8mA
This is a much more realistic situation for driving any external load, so you
should always refer the load to Vdd and drive the pin low to turn on the load,
rather than referring the load to ground and trying to drive the pin high.

In any case the part shouldn't sink more than 10mA per pin.

Tags: aduc8xx aduc8x aduc842
  • Share
  • History
  • More