Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC84x, tolerance of PLL output frequency
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • -ADuC84x: FAQ
    • ADuC84x, tolerance of PLL output frequency
    • ADuC84X. About ADuC84x external memory debug
    • ADUC84x: What state are the port pins set to, when the device is using the factory installed bootloader?
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC84x, tolerance of PLL output frequency

Q 

I am using ADUC843 with 32768 Hz crystal. The PLL is configured as it generates
16,78Mhz output. What is the tolarance of PLL output frequency?

 

A 

The ADuC84x PLL will generate exactly 512 core clock cycles for each input
clock cycle from the 32768Hz crystal. The average frequency is therefore
exactly 512 times the XTAL frequency and is therefeore determined by the
frequency error on the XTAL.
The PLL will introduce a small amount of random jitter but this will not be
significant in the operation of the device. If the PLL is allowed to operate in
free-running mode i.e. there is no external crystal connected, then the
tolerance of the clock core frequency is +/-20%.

Tags: aduc8xx aduc8x aduc843
  • Share
  • History
  • More