Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC845: Use of P2.3 as GPIO while using SPI in master mode
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • -ADUC845: FAQ
    • ADuC845 interrupt priority handling
    • ADuC845  calibration
    • ADUC845: Cascading 16 bit counters T0 and T1
    • ADuC845: Mixing inputs
    • aduc845: QS Kit for development
    • ADuC845: Silicon revision and anomaly sheet
    • ADuC845: Use of P2.3 as GPIO while using SPI in master mode
    • ADuC845_ADC interrupt
    • Using the ADUC845 Quick Start Development kit for ADUC847 and ADUC848?
    • Can ADUC845 analogue supply be shut down leaving digital supply on?
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC845: Use of P2.3 as GPIO while using SPI in master mode

Q 

Can I use pin P2.3 in ADuC845 as a general purpose pin while using SPI in
master mode?

 

A 

Yes you can. The SS pin is only used when the part is used as an SPI slave
device.
If the part is used as a Master device then the SS functionality is not
required and P2.3 can be used according to the alternate options given in the
Datasheet...T2 input or standard digital port pin.

Tags: aduc8xx aduc8x aduc845