Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Dont Let Your Feedback Loop Fall FlatPart 2: Dynamic Response and Isolation Innovation!

    Introduction In isolated power supply systems, maintaining a stable output voltage under varying load conditions is essential for reliable operation. The...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC845: Silicon revision and anomaly sheet
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • -ADUC845: FAQ
    • ADuC845 interrupt priority handling
    • ADuC845  calibration
    • ADUC845: Cascading 16 bit counters T0 and T1
    • ADuC845: Mixing inputs
    • aduc845: QS Kit for development
    • ADuC845: Silicon revision and anomaly sheet
    • ADuC845: Use of P2.3 as GPIO while using SPI in master mode
    • ADuC845_ADC interrupt
    • Using the ADUC845 Quick Start Development kit for ADUC847 and ADUC848?
    • Can ADUC845 analogue supply be shut down leaving digital supply on?
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC845: Silicon revision and anomaly sheet

Q 

1) Which silicon revision is currently shipping for ADuC845?
2) In "Anomaly Sheet for Silicon Rev. C ADuC845" it says that ADC noise
performance degrades when CD < 3. Will this be corrected in future silicon
revisions? If so, when can such revisions be expected? If not, can you
specifiy/quantify how the performance is degraded with CD=0 and 1 for 5V
operation? 

 

A 

Please find the answer to your questions below.
1) Which silicon revision is currently shipping for ADuC845?
1. The silicon currently shipping is Rev C.

2) In "Anomaly Sheet for Silicon Rev. C ADuC845" it says that ADC noise
performance degrades when CD < 3. Will this be corrected in future silicon
revisions? If so, when can such revisions be expected? If not, can you
specifiy/quantify how the performance is degraded with CD=0 and 1 for 5V
operation?

2. The ADC noise errata relates to a potential (and I stress the word
potential) case where due to code the ADC clock and the core (instruction)
clock on the fast sigma-delta parts can coincide causing excessive digital
noise in the part.
Ideally the ADC and core clocks are delayed relative to one another to minimize
noise, however due to the nature of the fast core scheme this delay is
dependant on the number of instructions used around and during the ADC loop of
the program. Unfortunately this is extremely difficult to quantify (i.e. in
terms of the exact number of instructions and is very dependant on the
application). The one thing I would say is that in general a customer will
probably not see this issue. So far, with all the ADuC845/7/8's in circulation
no-one has reported this issue. We have been able to see it in the lab under
ideal conditions and when explicitly looking for it, but otherwise it is
difficult to reproduce.

The degradation can be varied if the condition is seen and depends on
the
relationship between the ADC and core clocks that are themselves dependant on
the instructions being executed. The attached plots show a typical example of
the type of response seen at CD=0 and CD=1 when the issue can be seen. This is
by no means exactly what a customer will see. This is what we could see on our
test setup given the conditions under which we tested it.

Tags: aduc8xx aduc8x aduc845