Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents aduc845: QS Kit for development
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • -ADUC845: FAQ
    • ADuC845 interrupt priority handling
    • ADuC845  calibration
    • ADUC845: Cascading 16 bit counters T0 and T1
    • ADuC845: Mixing inputs
    • aduc845: QS Kit for development
    • ADuC845: Silicon revision and anomaly sheet
    • ADuC845: Use of P2.3 as GPIO while using SPI in master mode
    • ADuC845_ADC interrupt
    • Using the ADUC845 Quick Start Development kit for ADUC847 and ADUC848?
    • Can ADUC845 analogue supply be shut down leaving digital supply on?
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

aduc845: QS Kit for development

Q 

1) If I purchase the QuickStart dev kit for the ADuC 845, could I also use it
to develop for the ADuC 847 (which is a subset of the 845)? Would their be any
limitations in doing this?

2) Does the Keil C-Compiler support the extended stack feature of these micros?

 

A 

1) If I purchase the QuickStart dev kit for the ADuC 845, could I also use it
to develop for the ADuC 847 (which is a subset of the 845)? Would their be any
limitations in doing this?

Yes, you can use the ADuC845 QS kit to develop for the ADuC847, or for that
matter the ADuC848. The only thing you must take account of is the difference
in the ADC specifications. Otherwise everything else is identical.
The ADuC845 incorporates two 24-bit ADCs (Primary and Auxiliary) whereas the
ADuC847 only has a single 24-bit ADC (Primary) and the ADuC848 has a single
16-bit ADC (Primary). Neither the ADuC847 nor the ADuC848 allow the use of the
temperature sensor due to the missing Auxiliary ADC.                 


2) Does the Keil C-Compiler support the extended stack feature of these micros?

Yes.

Tags: aduc8xx aduc8x aduc845