Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC845  calibration
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • -ADUC845: FAQ
    • ADuC845 interrupt priority handling
    • ADuC845  calibration
    • ADUC845: Cascading 16 bit counters T0 and T1
    • ADuC845: Mixing inputs
    • aduc845: QS Kit for development
    • ADuC845: Silicon revision and anomaly sheet
    • ADuC845: Use of P2.3 as GPIO while using SPI in master mode
    • ADuC845_ADC interrupt
    • Using the ADUC845 Quick Start Development kit for ADUC847 and ADUC848?
    • Can ADUC845 analogue supply be shut down leaving digital supply on?
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC845  calibration

Q 

Can you get the equation of the output code and calibration register? Like the
one in below of AD7793.
Unipolar:
Data = [ (0.75*Vin*PGA_Gain/Vref) * (2^23) - (Offset_Reg-800000h) ] *
Full_Scale_Reg/400000h * 2
Bipolar:
Data = [ (0.75*Vin*PGA_Gain/Vref) * (2^23) - (Offset_Reg-800000h) ] *
Full_Scale_Reg/400000h + 800000h
The nominal values of Offset_Reg is 800000h and of Full_Scale_Reg is 555555h.
The 0.75 number will vary slightly from part-to-part because of manufacturing
tolerances.

 

A 

The Gain register is a 24-bit number that adjusts the gain of the ADC transfer
function.
For example, if the GN0 register value is increased by +10%, then the ADC
result will also increase by +10%.
e.g. on the 2.56V range and bipolar coding, VIN=1.28V normally converts to
0xC00000.
If the GN0 register is increased by 10%, VIN=1.28V will convert to 0xC66666.


The Offset register is a little more complex to describe.
The basic function is that when the OF0 register is increased, the ADC0 DAT
register will decrease.
A value of 0x800000 in OF0 means no offset is removed.
However the weight of 1 LSB of OF0 is not equal to 1LSB of ADC0 DAT.
1 LSB of OF0 subtracts more that 1 LSB of ADC0 DAT.

This relationship is given by:  1 OF0 LSB is equal to (4 / 3.072) ADC0 DAT LSB.
This assumes that:
  (i) The ADC is in Bipolar mode (the UNI bit is equal to 0)
(ii) The PGA Range is not on the +/-20mV range.
(iii) The GN0 register is at its default value, i.e. it has not been modified
by a user System-Full-Scale calibration.

If the ADC uses Unipolar coding or the PGA Range = 20mV then 1 OF0 LSB weight
is 2X bigger.
If the ADC GN0 value is modified, then the weight of 1 OF0 LSB changes, because
the Gain scaling occurs after the ADC output is adjusted by the OF0 register.

Tags: aduc8xx aduc8x aduc845