Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC845_ADC interrupt
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • -ADUC845: FAQ
    • ADuC845 interrupt priority handling
    • ADuC845  calibration
    • ADUC845: Cascading 16 bit counters T0 and T1
    • ADuC845: Mixing inputs
    • aduc845: QS Kit for development
    • ADuC845: Silicon revision and anomaly sheet
    • ADuC845: Use of P2.3 as GPIO while using SPI in master mode
    • ADuC845_ADC interrupt
    • Using the ADUC845 Quick Start Development kit for ADUC847 and ADUC848?
    • Can ADUC845 analogue supply be shut down leaving digital supply on?
  • +ADuC847: FAQ
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC845_ADC interrupt

Q 

ADUC845 has two ADC core and I think they must can work at the same time.
But there is only one ADC interrupt and there is no explanation on our
datasheet for the issue below.
Would you kindly give the confirmation for the issue below. Many thanks!

 

A 

AD0CON1/2
Any write to this SFR during an active mode with AD0EN =1, and the main ADC has
not completed its single conversion / calibration, causes both ADCs to be
interrupted, and a new conversion / calibration to commence. The contents of
ADSTAT (except
NOXREF) are cleared when this occurs (This may take a number of machine cycles).
AD1CON
Any write to this SFR during an active mode with AD1EN = 1 causes the auxiliary
ADC to be interrupted, and a new conversion / calibration to commence. The
conversion
will not commence until the next chop edge if the main ADC is already
converting;
but if the main ADC has completed its single conversion / calibration then the
auxiliary ADC will re-start immediately. The RDY1 and ERR1 bits of ADSTAT are
cleared when this occurs. The CAL bit will also be cleared, unless the main ADC
has
just completed its single conversion / calibration.
ADMODE
Any writes to this SFR that involve a change in the MD bits, or set AD0EN, or
rewrite
the same information will cause both ADCs to be interrupted, and a new
conversion
/ calibration to be initiated.The contents of ADSTAT (except NOXREF) are
cleared when this occurs. When the ADC clears the MD bits, it will not clear
the MD bits until each enabled ADC has completed
its single conversion or calibration.

Tags: aduc8xx aduc8x aduc845
  • Share
  • History
  • More