Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADuC847: Crystal start up
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • -ADuC847: FAQ
    • ADuC847: Crystal start up
    • ADUC847: Detecting the stop condition in slave mode
    • ADUC847 External reference voltage range
    • ADuC847: Noise perfomance
    • ADuC847: Using aspire in debug run mode
    • Recommended programming socket for ADuC847
    • I tested ADuC847 Burnout current to detect the short/open circuit. But it doesn't work
    • Model on Eval board - flash and supply - EVAL-ADuC847
    • What is the maximum Source current, that port P2.5 and P2.6 can deliver?
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADuC847: Crystal start up

Q 

I'm using ADuC836 with 85SMX watch crystal and all is working fine. With the
same crystal and ADuC848/847 samples, the oscillation don't start. I try 3
samples but nothing. why? could oscillator section be different from 836 to
847/848 chip? could be that all the 3 samples are damaged?

 

A 

   There is no difference between the parts. If it is working on the 836 then
there is no reason why if shouldn't work on the 847.
One thing I will say though is that Roberto should ensure that there are no
capacitors (decoupling) used on the XTAL1 and XTAL2 pins. There is sufficient
internal capacitance to ensure oscillation.
Confirm that the crystal is indeed across XTAL1 and XTAL2 and that when the
part is powered up that oscillation can be seen on XTAL2.

This should be 32.768kHz. Do not load XTAL1 as this could damp the crystal
sufficiently to kill oscillation.
If XTAL2 is not oscillating (with the correct crystal connection and the part
powered up) then I would suggest that either

1. the part is not actually powered up correctly (the 836 and 847 are not pin
compatible)

2. the crystal is either faulty or is sufficiently far away such that the
impedance, parasitic capacitance and inherent inductance of the traces are
loading the crystal sufficiently to kill the oscillation.
The PLLCON SFR is only of use to select a particular core operating speed.

Tags: aduc8xx aduc8x aduc847