Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADUC847: Detecting the stop condition in slave mode
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • -ADuC847: FAQ
    • ADuC847: Crystal start up
    • ADUC847: Detecting the stop condition in slave mode
    • ADUC847 External reference voltage range
    • ADuC847: Noise perfomance
    • ADuC847: Using aspire in debug run mode
    • Recommended programming socket for ADuC847
    • I tested ADuC847 Burnout current to detect the short/open circuit. But it doesn't work
    • Model on Eval board - flash and supply - EVAL-ADuC847
    • What is the maximum Source current, that port P2.5 and P2.6 can deliver?
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADUC847: Detecting the stop condition in slave mode

Q 

I need technical informations about Analogue Device ADuc847

I want to use it in I2C hardware slave mode

Is it possible to detect I2C Stop sequence in software ?

The problem is when the master abort the communication sequence before the
normal end The slave couldn't detect de stop sequence in software point of view

 

A 

There is no register or indicator on the ADUC847 that you can read to tell that
the I2C interface has received a valid stop condition 

Note that the ADuc841/2 has a Stop detection(see p48 of datasheet, BIT7),
although the ADC is much different to the ADuc845.

Here are some notes that may help;


STOP CONDITION:

The I2CI interrupt bit (Bit 0) is set by the user every time the byte is
transmitted or received.

Bits I2CTX2 (Bit 2) will indicate whether the Micro-controller is transmitting
or receiving. I2CTX=0, means that the micro-controller is receiving.

From these 2 bits, we have the following: once the I2CTX = 0 ( receiving ) and
once the I2CI =1, then the byte has been received, the user can read the data
and the interrupt is cleared.

The interrupts will continue to occur while the data is being received. And
will continue to be cleared while the user reads the data. Once the user reads
the data and no interrupt occurs, then a STOP Condition has occurred. ( Timeout
will be required here, I’m not too sure how long ).

The only issue is that there is no guarantee that the last data byte is valid.
You will have to make that verification with software also. So care will be
needed.

From this also, the interface return to an IDLE state. So you are now sure what
state the controller is in.

Tags: aduc8xx aduc8x aduc847
  • Share
  • History
  • More