Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Other Products Library
    • Precision Technology Signal Chains Library
    • Software Modules and SDKs Library
    • Supervisory Circuits Library
    • Wireless Sensor Networks Library

    Latest Webinars

    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      KCC's Quizzes AQQ297 about taking the right dose of medication

      1. First, the quote of the month: " All my life I though air is free until I bought a bag of chips " - unknown 2. New quiz AQQ297 about taking the right...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Charting Calm Seas: Tips for Robust RS-485 Data Transmission

    by Bryson Barney As our world becomes ever more dependent on flawless digital communication, engineers need to find new ways of charting calm seas when...

     

    Unpacking IEC 61508: Low Complexity versus Type A Made Simple

    IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...

    Latest Blogs

    • Taming the AI Power Storm: Part 2 of 3
    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
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
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents I tested ADuC847 Burnout current to detect the short/open circuit. But it doesn't work
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • -ADuC847: FAQ
    • ADuC847: Crystal start up
    • ADUC847: Detecting the stop condition in slave mode
    • ADUC847 External reference voltage range
    • ADuC847: Noise perfomance
    • ADuC847: Using aspire in debug run mode
    • Recommended programming socket for ADuC847
    • I tested ADuC847 Burnout current to detect the short/open circuit. But it doesn't work
    • Model on Eval board - flash and supply - EVAL-ADuC847
    • What is the maximum Source current, that port P2.5 and P2.6 can deliver?
  • +ADUC848: FAQ
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

I tested ADuC847 Burnout current to detect the short/open circuit. But it doesn't work

Q 

I tested ADuC847 Burnout current to detect the short/open circuit. But it
deosn't work. And the ADuC847 Document said:
  "Burnout Current Enable Bit.When set, this bit enables the sensor burnout
current sources on primary ADC channels AIN4/AIN5 or AIN6/AIN7. Not available
on any other ADC input pins or on the auxiliary ADC (ADuC845 only)."
  I dont understand that "AIN4/AIN5 or AIN6/AIN7",these are not pairs of
differential input channels, the channels should be "AIN1/AIN2, AIN3/AIN4,
AIN5/AIn6, AIN7/AIN8", can you explain how does it work?

 

A 

You are correct, there is a typo on the datasheet that is being corrected. I
am currently waiting for website to be updated with latest datasheet.
In the meantime the correct pin outs for the burnout currents is as
follows....Ain5/6 and Ain7/8.
The current generated is 200uA from each burnout source, therefore the test
this you simply need to monitor the current either directly or by the voltage
drop across a resistor. The way the burnout detect circuit works is described
on page 32 of the datasheet. Simply put it says that if the sensor goes open
circuit then the ADC will read full-scale (i.e. V=IxR where R = infinite)  and
where the sensor has shorted the voltage read will be 0 (again V=IxR where R =
0).

Tags: aduc8xx aduc8x aduc847
  • Share
  • History
  • More