Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents ADUC848: Converting a small bipolar signal.
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • -ADUC848: FAQ
    • My customer has some technical problems/questions about ADuC848.
    • ADUC848: Configuration of current source IEXC[0|1]
    • ADUC848: Converting a small bipolar signal.
    • ADUC848: Is there a single device with supply range 2.7 to 5.5 V?
    • Aduc848: Verify in hardware that program has been succesfully load into chip
    • Which is the maximum value of the external clock  for the PWM on ADuc848?
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

ADUC848: Converting a small bipolar signal.

Q 

I have external reference 2,5V, ADR441, and I need to measure voltages in the
range of +-80mV. Is it possible to do if the signal from my source is going to
AIN1 and  AINCOM or does it need go to AIN1 and AIN2?

 

A 

You need to convert a bipolar signal (+/-80mV). The ADuC848 cannot measure
voltages that go 80mV below GND so if your +/-80mV source is referred to Ground
you will have a problem interfacing directly to the ADuC848.

Usually, such small signals come either from a resistive "wheatstone" bridge
(as shown connected to pins 15 and 16 in figure 71 page 93 of ADUC848
datasheet, or from a sensor which can be biased at a voltage above ground
(thermocouple, RTD). In both of these cases the differential voltage can be
e.g.  +/-80mV but the common mode voltage lies between VDD and ground.

For a wheatstone bridge, you would normally use a fully differential connection
(signal connected between AIN1 and AIN2 for example)

For a floating sensor, you can either use a fully differential connection or a
pseudo-differential connection (signal connected between AIN1 and AINCOM).

In both these cases, all the input voltages need to lie between GND and AVDD at
all times. If you use the on-chip buffer, there is an additional constraint
that the absolute voltage on AIN1 and AIN2,AINCOM must remain in the range AGND
+ 100mV to AVDD - 100mV.

Tags: aduc8xx aduc8x aduc848