Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Dont Let Your Feedback Loop Fall FlatPart 2: Dynamic Response and Isolation Innovation!

    Introduction In isolated power supply systems, maintaining a stable output voltage under varying load conditions is essential for reliable operation. The...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents My customer has some technical problems/questions about ADuC848.
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • -ADUC848: FAQ
    • My customer has some technical problems/questions about ADuC848.
    • ADUC848: Configuration of current source IEXC[0|1]
    • ADUC848: Converting a small bipolar signal.
    • ADUC848: Is there a single device with supply range 2.7 to 5.5 V?
    • Aduc848: Verify in hardware that program has been succesfully load into chip
    • Which is the maximum value of the external clock  for the PWM on ADuc848?
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

My customer has some technical problems/questions about ADuC848.

Q 

My customer  has some technical problems/questions about ADuC848.

They used ADuC836 earlier but now trying to use ADuC848BS62-5. They save
content of the RAM (60 byte/ 15 page) at the EEPROM data memory when power
down. They
did not have any problem with ADuC836 but they can save only 20 byte / 5 page
using ADuC848. And, they need our help to solve the problem.

Please find some working informations below.

Supply voltage (DVdd, AVdd) : 5 Volts
Capacitor connected to power supply : 470 micro Farads
Only ADuC848 draws required currents, the others no.
PLLCON = 00000001B ( Core Clock = 6.29 MHz )
PSMCON = 11000001B ( DVdd, AVdd trip point = 4,63V )

FLASH/EE Data-Memory erased when power-on.

Only write operation done When PSM-INTERRUPT accepted.

 

A 

When the system supply is removed, the Power Supply Monitor (set to 4.63V)
triggers an interrupt which starts the subroutine to save the RAM values to
EEPROM data memory.

The difference between the ADuC848 and the ADuC836 in this regard is that the
ADuC848 comes in two voltage grades, 3V and 5V indicated by the -3 ro -5 at the
end of the part number.

The 5V part, which you are using, has a hardware power-on reset circuit whose
threshold is fixed at 4.63V.

Since the highest threshold for the power supply monitor is also 4.63V, the
Power supply Monitor function cannot be used with the 5V version of the ADuC848
- see page 68 of the ADuC848 datasheet. In fact the part will receive a
hardware reset at around the same voltage as the Power supply monitor is
triggered so there will be little or no time for any last minute processing to
take place.

A common solution, to receive advanced warning of a power down event, is to
obtain the interrupt signal from BEFORE the voltage regulator. Devices like our
ADM708 obtain a power fail signal from before the regulator and therefore give
you some extra time to store the RAM values into EEPROM.

Tags: aduc8xx aduc8x aduc848