Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
8052 Core Products
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
8052 Core Products
  • Processors & Microcontrollers
8052 Core Products
Documents Aduc848: Verify in hardware that program has been succesfully load into chip
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADuC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADuC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADuC836: FAQ
  • +ADuC83x: FAQ
  • +ADUC841: FAQ
  • +ADuC842: FAQ
  • +ADUC845: FAQ
  • +ADuC847: FAQ
  • -ADUC848: FAQ
    • My customer has some technical problems/questions about ADuC848.
    • ADUC848: Configuration of current source IEXC[0|1]
    • ADUC848: Converting a small bipolar signal.
    • ADUC848: Is there a single device with supply range 2.7 to 5.5 V?
    • Aduc848: Verify in hardware that program has been succesfully load into chip
    • Which is the maximum value of the external clock  for the PWM on ADuc848?
  • +ADuC84x: FAQ
  • +ADUC8xx: FAQ
  • +ADUCXX: FAQ

Aduc848: Verify in hardware that program has been succesfully load into chip

Q 

My question is after I have program the aduc848 chip, how can I verify whether
the program is successfully loaded into the chip? Is there any pin on the
aduc848 will show indication (may be the pin will go high or low, after
successfully program the chip)?

 

A 

Firstly, the device is put into Kernel mode if PSEN is low at the time the
RESET signal is released. If the part goes into  kerne mode successfully, PSEN
is ignored from that point onwards.

If you are using the DOS downloader to download code to the device, there will
be a confirmation of the success or otherwise of the download operation which
is shown on the screen.

I don't know of a reliable hardware method to detect whether the transfer is
successful. You can always supervise the activity on the UART - when it stops
then the transfer is complete.

However there is some error checking etc that goes on as part of the serial
download protocol, and this is what the command line debugger looks for, before
asserting that the download was successful. After each datapacket sent by the
PC to the ADuC848, the ADuC848 should respond with an ACK code <06h> or the
NACK code <07h> if there is some problem (incorrect checksum, internal failure
to carry out the requested instruction). See the attached description of the
serial download protocol for details. If your tester is smart enough to detect
these ACK or NACK signals then this would allow you to determine not only if
the download is complete but also if there were any errors during the download
procedure.

Tags: aduc8xx aduc8x aduc848