Post Go back to editing

FT232 interface with ADuCM3029

Thread Summary

The user asked if interfacing an FT232 operating at 3.3V with an ADuCM3029 operating at 3V would cause issues. The final answer states that the ADuCM3029 can operate up to 3.6V, so 3.3V is safe. The GPIOs have internal ESD protection diodes, which will not conduct with a 0.3V difference, ensuring no problems with the interface.
AI Generated Content

We are interfacing FT232 to aducm3029 which operates at 3V. But the FT232 operates at 3.3V . Will this cause a problem?

Thread Notes