Post Go back to editing

ADuC847 freezing

Category: Hardware
Product Number: ADUC847

Hi there! 

I've been using the ADuC847 in my equipments for a while and it works great. Basically i use it to read a load cell and do some I/O depending on the weigh i'm reading. The problem is that in some cases the CPU just stops working, it freezes and need a hard reset, but i can't do that since my equipments need to be running without stop. 

It seems to be a problem regarding the power supply or grounding, but i still didn't find a definitive solution, not even the WDT solves it 100%. 

Can anyone here help me with this? 

Parents
  • Hi Henrique,

    Is the device freezing limited to only a few devices or all of the device you're using are freezing after a certain period? How long before it freezes?

    After the hard reset, does the device freeze immediately or after a certain period?

    If there's a problem with the power supply, we can try using the power supply monitor, to check if the supply is going below the recommended operating level.

    Regards,

    Karl

  • Hi Karl! 

    Every device freezes, but it depends on where it is. I believe it's a power supply issue, but on the AC power suppply so the power supply monitor doesn't catches this effect. It can also be regarding the ground. 

    After the hard reset it freezes after a certain period, but it's not always the same period. 

Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.