Post Go back to editing

ADuC847 freezing

Category: Hardware
Product Number: ADUC847

Hi there! 

I've been using the ADuC847 in my equipments for a while and it works great. Basically i use it to read a load cell and do some I/O depending on the weigh i'm reading. The problem is that in some cases the CPU just stops working, it freezes and need a hard reset, but i can't do that since my equipments need to be running without stop. 

It seems to be a problem regarding the power supply or grounding, but i still didn't find a definitive solution, not even the WDT solves it 100%. 

Can anyone here help me with this?