ADuCM3029
Recommended for New Designs
The ADuCM3027/ADuCM3029 microcontroller units (MCUs) are ultra low power microcontroller systems with integrated power management for processing, control...
Datasheet
ADuCM3029 on Analog.com
I tried several times to use SensorPal to connect to the EVAL-ADICUP3029, but it didn't work.
The USB is selected on the three was UART swtich (S2) and the switch S5 is in the "Wall/USB" position.
The Output display shows the following errors:
Furthermore, it displays me the 'FAIL.TXT' saying 'The interface firmware FAILED to reset/halt the target MCU'.
I tried to dran and drop the ADICUP3029 Interface file as explained under the section "Maintenance Drive" on this page ADICUP3029 PC/Laptop Drivers [Analog Devices Wiki].
I tried to erase the flash using the CrossCore Serial Flash Programmer but it didn't work.
It just displays me this:
"Sending second stage kernel.
Read Intel HEX application image with 668 bytes.
No autobaud response."
I tried again to update the firmware on the board using SensorPal but I alway get the same error (explained before).
stephenv - Moved from Other Products (EN) to 8052 Core Products. Post date updated from Monday, November 18, 2024 9:59 AM UTC to Tuesday, February 3, 2026 9:09 PM UTC to reflect the move.