Post Go back to editing

Urgent! Regarding MAX32660 GPIO interrupt issue

Thread Summary

The user inquires about using PB_11/UART2_Rx or P0.5/UART0_Rx as a GPIO interrupt input to wake up the MAX32660 MCU from low-power modes. The final answer directs the user to Analog Devices' technical support pages for further assistance and suggests reviewing a related FAQ. The accompanying answer clarifies the need for a wake-up interrupt pin.
AI Generated Content
Category: Software
Product Number: MAX32660

Dear Support,

Please help me.

Regarding MAX32660 GPIO interrupt issue, Can I use PB_11/UART2_Rx pin as GPIO interrupt input?

If no, could you please recommend one pin for gpio interrupt to me? 

Thanks for your support.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.