Post Go back to editing

Program code for Tunable laser design with ADuC834

Thread Summary

The user inquired about the program code and BOM for a tunable laser reference design using ADuC834, ADN8830, and ADN2830 (AN-655). The support engineer indicated that while no specific tunable laser program is available, the ADuC8XX installer includes documentation and example programs, and the AN-655 document contains an Assembly Language program. The BOM for the module is not available online.
AI Generated Content

Hiii...... 

Does any one have program code of the module used in tunable laser reference design for designers with ADuC834, ADN8830, ADN2830 (AN-655)..?

and any one have BOM of module used.??

  • Hi,

    I guess that this is more a question for the 8052 Core Products community.

    Thanks,
    Dragos

  • Hi Varma,

    We don't have a specific example program dedicated for Tunable laser application. The installer for ADuC8XX includes documentations, example program to run a certain block. I also checked AN-655 and I believe it does include a program written in Assembly Language which can be found on this section of the document "ADuC832 SOFTWARE".

    In case you still need the documentations and sample programs, here is the link where you can download them: ADuC8XX

    Unfortunately for the BOM, it is not posted on the web and I cannot locate them too.

    Hope this helps Varma.

    Thanks!

    Regards,

    AJ