Post Go back to editing

Reading Temperature from ADUCM360 from CN0359 Kit Problem

in EVAL-CN0359-EB1Z Open source code ,  we want to change the adc1  to read the Internal Temp Sensor inside the ADUCM360 .

 

We do the changes in the below ,  But the code is not working. Temp value is coming so incorrect and with - Values ( Like -29 C , -17 C )

 

static int on_adc1(int argc, char *argv[])

{

                float fVolts   = (1.2 / 268435456);      // Internal reference, calculate lsb size in volts

                float fVoltage = (adc1_result * fVolts);// Calculate ADC result in volts

                float internal_temperature = 25.0 - (((fVoltage * 1000.0) - 82.1) * 4.0);

 

pADI_ADC1->CON = (pADI_ADC1->CON & ~ADCCON_BUFBYPN_MSK & ~ADCCON_BUFBYPP_MSK & ~ADCCON_BUFPOWN_MSK & ~ADCCON_BUFPOWP_MSK & ~ADCCON_ADCCODE_MSK & ~ADCCON_ADCREF_MSK & ~ADCCON_ADCCN_MSK & ~ADCCON_ADCCP_MSK) | ADCCON_BUFBYPN | ADCCON_BUFBYPP | ADCCON_BUFPOWP | ADCCON_BUFPOWN | ADCCON_ADCCODE_INT | ADCCON_ADCREF_INTREF | ADCCON_ADCCN_TEMP | ADCCON_ADCCP_TEMP;

                pADI_ADC1->ADCCFG = (pADI_ADC1->ADCCFG & ~ADCCFG_EXTBUF_MSK) | ADCCFG_EXTBUF_OFF;

                pADI_ADC1->MDE = (pADI_ADC1->MDE & ~ADCMDE_PGA_MSK) | ADCMDE_PGA_G2;

                pADI_ADC1->MSKI = (pADI_ADC1->MSKI & ~ADC1MSKI_RDY_MSK) | ADCMSKI_RDY_EN;

 

                ADC1CON_ADCEN_BBA = true;

 

                return 0;

}

Please help us to fix this problem.

Regards...

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.