Article ADUC834: Can I use analog inputs on Port 1 pins for digital I/0?

Q 

Port 1 on the ADuC834 is primarily used for analog inputs. Can I use Port 1
pins for digital I/0?
If so, how?

 

A 

Pins 1.2 to P1.7 inclusive are analog input/digital input pins. They have no
digital output
capabilities. The default configuration for these six Port 1 pins is as analog
inputs. In the default
state, the Port 1 register contains FFh. To configure any of these six Port 1
pins as a digital input,
simply clear the corresponding bit to zero in the Port 1 register (P1).
P1.0 and P1.1 are digital I/O pins and have a pull-up configuration as
described in datasheet for Port 3.
Both P1.0 and P1.1 have an increased current sink capability of 10 mA.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.