Q
The MicroConverter has separate pins for analog and digital grounds. Should I connect these to two separate ground planes on my board?
A
No. At least, not unless the two ground planes are connected…
Q
Can you please supply the specification for the on-board temperature sensor on the ADUC824/ADUC834 devices? I need an accurate description of the temp channel. This doesn't appear in the datasheets…
Q
The primary ADC is differential. Can I convert on a single-ended input voltage by grounding one of the inputs?.
A
No, the ADC inputs for the primary ADC cannot be within 100mV of the rails. Hence…
Q
Port 1 on the ADuC834 is primarily used for analog inputs. Can I use Port 1 pins for digital I/0? If so, how?
A
Pins 1.2 to P1.7 inclusive are analog input/digital input pins. They have no digital…
Q
Will I need to implement an external reset generator circuit for my ADuC834 design?
A
No, you will not have to implement an external reset generator. The ADuC834 has an integrated robust power…
Q
Does changing the PLL divider value via the CD bits in PLLCON affect the baud rate?
A
Yes, changing the CD bits does affect the baud rate. The output of the PLL divider is the core clock frequency…
Q
I want to drive LEDs directly from some digital outputs what pins should I use?
A
The high drive port pins are P1.0 and P1.1. Both of these port pins are tested to sink 10mA and keep the VOL…
Q
How do I configure the ADuC834 UART serial port at 9600/115200 baud?
A
The UART serial port on the ADuC834 can be configured for 9600 baud using the following piece of code (assuming CD in PLLCON…
Q
How do I use the on-chip temperature sensor feature of the ADuC834?
A
The temperature sensor on the ADuC834 is converted by the auxiliary ADC to output a digital code to represent the chip temperature…
Q
ADuC834: I am changing ranges and I am seeing much more than 2uV gain mis-match. Why?
A
You should not see much more than 2uV gain matching. i.e. as you changes the range from one range to another…