Q
Can I program Port 1 and 3 as input or output, ie is it to send logic 1 or logic 0 via port 1 and 3? In the document, it says, whenever you write 0, it becomes input. It also says P1.2-P1.7 cannot…
Q
In the ADuC814 datasheet, it is mentioned that the internal temperature sensor of ADuC8xx gives 650mV at 25C and that "is a voltage output ... which is proportional to absolute temperature". What is…
Q
The output of the temperature sensor is different (quite a lot) than that is mentioned in the datasheet for room temperature. May the sensor be broken down or do I have to make calibration? If so,…
Q
Got the ADuC841 MicroConverter SAR Evaluation Board Rev.A4 delivered but there only seem schematics for Rev. A3 ( https://www.analog.com/media/en/technical-documentation/evaluation-documentation/151851ADuC_SAR_PCB_A3…
Q
For ADUC814, what is the minimum time and level of the reset impulse I need to ensure a CPU reset? VDD is 4V.
A
The ADuC814 is specified for DVdd supply of 3V/5V (3V +/-10% and 5V +/-10%). We…