KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Dear developer, dear support,
I'm working on ZedBoard + FMCOMMS2 + AD9361. I'm new with AD9361. (I'm new with support community, sorry if the discussion is not in the correct section) I have to develop a project with this transceiver and I a started with the ADI reference design, HDL for FPGA part and No-OS for software/driver. For HDL I started with the original one and I modified it according to the requirements of the new project. Especially, I removed the ADC and DAC part, the DMA and VDMA management and I added an IP for data modulation/demodulation. This IP communicate to PS of Zynq via AXI-Lite. In the software no-OS (baremetal application), I modified the software accordingly: I removed driver for ADC - DAC. Now I created my application and I'm able to communicate via AXI between PS and PL, I configure correctly the IP, and the init of AD9361 with ad9361_init seems to be accomplished successfully. But I'm not able to configure correctly the rate of the various clock of AD9361. I need the CLK_OUT = 40 MHz (used as a reference clock in the FPGA design) and the ADC_CLK = 160 MHz in order to have a 40 MSps in LVDS configuration. I have 1 rx channel and 1 tx channel. I'm using in loop-back configuration with a SMA-SMA cable between the TX1A (J112) and RX1A (J110). I set the REG_BBPLL in the following way:
| #define CLKOUT_ENABLE | (1 << 4) /* CLKOUT Enable */ | ||
| #define DAC_CLK_DIV2 | (1 << 3) /* DAC Clk div2 */ |
| #define CLKOUT_SELECT(x) | (((x) & 0x3) << 5) /* CLKOUT Select<2:0> */ | |
| #define BBPLL_DIVIDER | (((x) & 0x2) << 2) /* BBPLL Divider <2:0> */ |
in order to have CLKOUT=ADC_CLK/4. Even if BBPLL_DIVIDER is not used in the init.
As init parameters, I used the default AD9361_InitParam default_init_param except for the following part:
| /* Base Configuration */ | |||
| 0, | //two_rx_two_tx_mode_enable *** adi,2rx-2tx-mode-enable |
/* Rate & BW Control */
{720000000, 160000000, 80000000, 40000000, 40000000, 40000000},//uint32_t rx_path_clock_frequencies[6] *** adi,rx-path-clock-frequencies
{720000000, 160000000, 80000000, 40000000, 40000000, 40000000},//uint32_t tx_path_clock_frequencies[6] *** adi,tx-path-clock-frequencies
| CLKOUT_ENABLE, | //clk_output_mode_select *** adi,clk-output-mode-select |
In this way, I figured to set BBPLL as a 720 MHz clock, the ADC and DAC clock 160 MHz (for LVDS config) that sustain a 40 MSPS. Is it correct? But if I check the CLK_OUT frequency in P202 test-point I find the frequency is 45 MHz, then I can think the ADC_CLK is 180 MHz. In fact, if in the consolle I get tx_samp_freq? and rx_samp_freq? i receive 45 MHz. If i set rx_samp_freq=40MHz the CLK_OUT measured is 80 MHz. Is it possible? The ADC_CLK should be 320 MHz? At the init, the register 0x00A is set to 0x72, I'm not able to set the D3 bit to 1, and after the set command rx_samp_freq=40MHz 0x00A register is 0x79. Is there something wrong in this configuration? How can i set the ADC/DAC clock is 160 MHz and consequently the CLK_OUT = 40 MHz? Or I have just to set the register 0x00A to 0x12 (just to have buffered version of DCXO 40 MHz)? What is the correct step or procedure to correctly initialize the AD9361 with the desired rate?
Thank you in advance for your attention,
Gab
Hi Gabriele,
{720000000, 160000000, 80000000, 40000000, 40000000, 40000000}, // rx-path-clock-frequencies
{720000000, 160000000, 80000000, 40000000, 40000000, 40000000}, // tx-path-clock-frequencies
is an invalid option. If you want a 40 MSPS rate, then some valid options are:
rx_path_clks = 1280000000, 320000000, 160000000, 80000000, 40000000, 40000000
tx_path_clks = 1280000000, 320000000, 160000000, 80000000, 40000000, 40000000
or
rx_path_clks = 960000000, 480000000, 160000000, 80000000, 40000000, 40000000
tx_path_clks = 960000000, 240000000, 80000000, 80000000, 40000000, 40000000
For example, setting:
{1280000000, 320000000, 160000000, 80000000, 40000000, 40000000}, // rx_path_clock_frequencies[6]
{1280000000, 320000000, 160000000, 80000000, 40000000, 40000000}, // tx_path_clock_frequencies[6]
ADC_CLK_DIV_8, // clk_output_mode_select
should provide you a 40 MHz CLK_OUT.
Regards,
Dragos
You configuration was invalid since 720/160 = 4.5 !
And 160 * 4 = 640,
640 != 720
In 1Rx1Tx mode DATA_CLK = 2 * IQ_RATE
In 2Rx2Tx mode DATA_CLK = 4 * IQ_RATE
-Michael
BTW - Please use the API functions to set the sample (IQ_Rate) rates.
There is no good reason to calculate these rates manually.
The driver will do it for you.
-Michael
Hi Dragos
first of all, thank you very much for your kind and quick reply.
I just tried both configuration you proposed me and effectively they are both working properly. By setting ADC_CLK/8, I have CLK_OUT=40 MHz. I'd like to ask you, but I don't want to waste your time, why my configuration was invalid. I figured to set the rx and tx chain as reported in the attachedd pics (following a previous thread you posted some times ago). In any case, now it's working, and if I get command configuration rx_samp_freq? and tx_samp_freq? both of them get 40 MHz.
Just some more clarification. For debug purpose, I routed the internal clock to zedboard pmod. In particular, the single-ended version of rx_clk_in_p and rx_clk_in_n, that is DATA_CLK, is it correct? In the case I set
| 0, | //two_rx_two_tx_mode_enable *** adi,2rx-2tx-mode-enable |
this clock is 80 MHz.
If
| 1, | //two_rx_two_tx_mode_enable *** adi,2rx-2tx-mode-enable |
this clock is 160 MHz. Right? Then, if I need to have a 1:4 ratio between DATA_CLK and CLK_OUT, I have to set two_rx_two_tx_mode_enable set to 1 even if I have only one channel. Is it correct?
Thanks in advance for your attention.
Best regards,
Gabriele
Hi Gabriele,
The initialization parameters will be set in the AD9361_InitParam. Some of the settings can be changed during run time using the API functions: https://github.com/analogdevicesinc/no-OS/blob/master/ad9361/sw/ad9361_api.h#L355
Regards,
Dragos
Gabriele, yes, this is correct.
Regards,
Dragos
Thank you Michael for your reply. Now it is evident where is my error.
All the parameters I need to set are in AD9361_InitParam?
Gabriele
Hi Dragos,
thanks. I'm working with this API. At the moment I need just to manage AD9361_InitParam. But for instance, If I need to change at run time the rate paths I should utilize ad9361_set_trx_path_clks, or if I want to change the initial rf_rx_bandwidth_hz I should use ad9361_get_rx_rf_bandwidth. And so on. Correct?
Thanks a lot for your explanations,
Gabriele