I am using the AD9172 FMC evaluation board in order to generate SPOT frequencies ranging from 2 to 3.5 GHz. I have successfully migrated the ADI reference design available for the VCU to a ZCU102 with micro-blaze (PL SIde). I am also able to build the vitis application (2023.2) using ADI's no os guide however during the debug process i am getting the following error:
WARNING : Read/Write check failed (0xFF)
Probed. SPI read support failed
tx adxcvr : OK (7372800 kHz)
The execution is stuck in a while loop and the jesd link does not become active
I have made sure to check all physical constraints related to spi properly wrt to zcu102 and i am also able to observer the spi_mosi, spi_sclk, spi_cs on the pmod header as well as in the iLA.
It looks like there is some issue in the read/response (spi_miso) from the hmc7044.
I have also verified the axi quad spi IP attributes and setting and made sure that the io1_i, io1_o, io0_i, io0_o assignments are proper.
I am using a very low SPI clock of 1.5625 MHz

I can also confirm that there is nothing wrong with the zcu102 carrier board since the zynq PS design for the ad9172 is working perfectly fine.
I am attaching my top.v file below
`timescale 1ns/100ps
module system_top #(
parameter NUM_LINKS = 2,
parameter DEVICE_CODE = 0
) (
input sys_rst,
input USER_SI570_P,
input USER_SI570_N,
input uart_sin,
output uart_sout,
output c0_ddr4_act_n,
output [16:0] c0_ddr4_adr,
output [ 1:0] c0_ddr4_ba,
output [ 0:0] c0_ddr4_bg,
output [ 0:0] c0_ddr4_ck_c,
output [ 0:0] c0_ddr4_ck_t,
// output ddr4_ck_p,
// output ddr4_ck_n,
output [ 0:0] c0_ddr4_cke,
output [ 0:0] c0_ddr4_cs_n,
inout [ 1:0] c0_ddr4_dm_dbi_n,
inout [15:0] c0_ddr4_dq,
inout [ 1:0] c0_ddr4_dqs_c,
inout [ 1:0] c0_ddr4_dqs_t,
output [ 0:0] c0_ddr4_odt,
output c0_ddr4_reset_n,
// output mdio_mdc,
// inout mdio_mdio,
// input phy_clk_p,
// input phy_clk_n,
// output phy_rst_n,
input ETH_0_RXN,
input ETH_0_RXP,
output ETH_0_TXN,
output ETH_0_TXP,
output [1:0] SFPx_TX_DISABLE,
inout [16:0] gpio_bd,
output gpio_1,
output gpio_2,
input gpio_3,
input gpio_4,
//output iic_rstn,
inout iic_scl,
inout iic_sda,
input SFP_SI5328_OUT_C_N,
input SFP_SI5328_OUT_C_P,
input USER_MGT_SI570_CLOCK2_P,
input USER_MGT_SI570_CLOCK2_N,
input tx_ref_clk_n,
input tx_ref_clk_p,
input tx_sysref_p,
input tx_sysref_n,
input [ 1:0] tx_sync_p,
input [ 1:0] tx_sync_n,
output [ 7:0] tx_data_p,
output [ 7:0] tx_data_n,
output spi_csn_dac,
output spi_csn_clk,
output spi_csn_clk2,
input spi_miso,
output spi_mosi,
output spi_clk,
output spi_en,
output PMOD0_0,
output PMOD0_1,
input PMOD0_2,
output PMOD0_3,
output PMOD0_4,
output PMOD0_5,
input PMOD0_6,
output PMOD0_7,
output PMOD1_0,
output PMOD1_1,
input PMOD1_2,
output PMOD1_3,
output PMOD1_4,
output PMOD1_5,
output PMOD1_6,
output PMOD1_7,
inout [ 4:0] dac_ctrl
);
// internal signals
wire [63:0] gpio_i;
wire [63:0] gpio_o;
wire [63:0] gpio_t;
wire [ 2:0] spi_csn;
wire tx_ref_clk;
wire tx_sysref;
wire [ 1:0] tx_sync;
wire tx_sysref_loc;
wire spi_clk_mon;
wire spi_miso_mon;
wire spi_mosi_mon;
// assign iic_rstn = 1'b1;
// spi
assign PMOD1_4 = spi_csn[0];
assign PMOD1_5 = spi_clk_mon;
assign spi_miso_mon = spi_miso;
assign PMOD1_6 = spi_miso_mon;
assign PMOD1_7 = spi_mosi_mon;
assign spi_clk = spi_clk_mon;
// assign spi_miso = spi_miso_mon;
assign spi_mosi = spi_mosi_mon;
// spi_en is active ...
// ... high for AD9135-FMC-EBZ, AD9136-FMC-EBZ, AD9144-FMC-EBZ,
// ... low for AD9171-FMC-EBZ, AD9172-FMC-EBZ, AD9173-FMC-EBZ
// If you are planning to build a bitstream for just one of those boards you
// can hardwire the logic level here.
//
assign spi_en = (DEVICE_CODE <= 2);
assign SFPx_TX_DISABLE = "11";
// 9135/9144/9172 916(1,2,3,4)
// 9135/9144/9172 916(1,2,3,4)
assign spi_csn_dac = spi_csn[1];
assign spi_csn_clk = spi_csn[0]; // HMC7044 AD9508
assign spi_csn_clk2 = spi_csn[2]; // NC ADF4355
/* JESD204 clocks and control signals */
// IBUFDS_GTE3 i_ibufds_tx_ref_clk_121 (
// .CEB (1'd0),
// .I (USER_MGT_SI570_CLOCK2_P),
// .IB (USER_MGT_SI570_CLOCK2_N),
// .O (tx_ref_clk_156),
// .ODIV2 ());
IBUFDS_GTE4 #(
.REFCLK_EN_TX_PATH(1'b0), // Refer to Transceiver User Guide.
.REFCLK_HROW_CK_SEL(2'b00), // Refer to Transceiver User Guide.
.REFCLK_ICNTL_RX(2'b00) // Refer to Transceiver User Guide.
)
IBUFDS_GTE4_inst (
.O(tx_ref_clk_156), // 1-bit output: Refer to Transceiver User Guide.
.ODIV2(), // 1-bit output: Refer to Transceiver User Guide.
.CEB(1'd0), // 1-bit input: Refer to Transceiver User Guide.
.I(tx_ref_clk_p), // 1-bit input: Refer to Transceiver User Guide.
.IB(tx_ref_clk_n) // 1-bit input: Refer to Transceiver User Guide.
);
// IBUFDS_GTE4 #(
// .REFCLK_EN_TX_PATH(1'b0), // Refer to Transceiver User Guide.
// .REFCLK_HROW_CK_SEL(2'b00), // Refer to Transceiver User Guide.
// .REFCLK_ICNTL_RX(2'b00) // Refer to Transceiver User Guide.
// )
// IBUFDS_GTE4_inst_1 (
// .O(mgt_ref_clk), // 1-bit output: Refer to Transceiver User Guide.
// .ODIV2(), // 1-bit output: Refer to Transceiver User Guide.
// .CEB(1'd0), // 1-bit input: Refer to Transceiver User Guide.
// .I(SFP_SI5328_OUT_C_P), // 1-bit input: Refer to Transceiver User Guide.
// .IB(SFP_SI5328_OUT_C_N) // 1-bit input: Refer to Transceiver User Guide.
// );
// IBUFDS_GTE3 i_ibufds_tx_ref_clk_126 (
// .CEB (1'd0),
// .I (tx_ref_clk_126_p),
// .IB (tx_ref_clk_126_n),
// .O (tx_ref_clk_126),
// .ODIV2 ());
IBUFDS i_ibufds_tx_sysref (
.I (tx_sysref_p),
.IB (tx_sysref_n),
.O (tx_sysref));
IBUFDS i_ibufds_tx_sync_0 (
.I (tx_sync_p[0]),
.IB (tx_sync_n[0]),
.O (tx_sync[0]));
IBUFDS i_ibufds_tx_sync_1 (
.I (tx_sync_p[1]),
.IB (tx_sync_n[1]),
.O (tx_sync[1]));
/* FMC GPIOs */
ad_iobuf #(
.DATA_WIDTH(5)
) i_iobuf (
.dio_t (gpio_t[21+:5]),
.dio_i (gpio_o[21+:5]),
.dio_o (gpio_i[21+:5]),
.dio_p ({
dac_ctrl /* 25 - 21 */
}));
/*
* Control signals for different FMC boards:
*
* dac_ctrl FMC 9144 like 9162 like 9172 like
* 0 H13 FMC_TXEN_0 FMC_TXEN_0 FMC_PE_CTRL
* 1 C10 NC NC FMC_TXEN_0
* 2 C11 NC NC FMC_TXEN_1
* 3 H14 FMC_TXEN_1 NC NC
* 4 D15 NC FMC_HMC849VCTL NC
*/
assign dac_fifo_bypass = gpio_o[40];
/* Board GPIOS. Buttons, LEDs, etc... */
ad_iobuf #(
.DATA_WIDTH(17)
) i_iobuf_bd (
.dio_t (gpio_t[0+:17]),
.dio_i (gpio_o[0+:17]),
.dio_o (gpio_i[0+:17]),
.dio_p (gpio_bd));
assign gpio_i[63:26] = gpio_o[63:26];
assign gpio_i[20:17] = gpio_o[20:17];
system_wrapper i_system_wrapper (
.PS_28V_STS_0(1'b1),
.PS_5V_LO_STS_0(1'b1),
.PS_5V_TX_STS_0(1'b1),
.SYNC_TRG_0(1'b1),
.ddr4_act_n (c0_ddr4_act_n),
.ddr4_adr (c0_ddr4_adr),
.ddr4_ba (c0_ddr4_ba),
.ddr4_bg (c0_ddr4_bg),
.ddr4_ck_c (c0_ddr4_ck_c),
.ddr4_ck_t (c0_ddr4_ck_t),
.ddr4_cke (c0_ddr4_cke),
// .ddr4_ck_c (ddr4_ck_n),
// .ddr4_ck_t (ddr4_ck_p),
// .ddr4_cke (c0_ddr4_cke),
.ddr4_cs_n (c0_ddr4_cs_n),
.ddr4_dm_n (c0_ddr4_dm_dbi_n),
.ddr4_dq (c0_ddr4_dq),
.ddr4_dqs_c (c0_ddr4_dqs_c),
.ddr4_dqs_t (c0_ddr4_dqs_t),
.ddr4_odt (c0_ddr4_odt),
.ddr4_reset_n (c0_ddr4_reset_n),
.gpio0_i (gpio_i[31:0]),
.gpio0_o (gpio_o[31:0]),
.gpio0_t (gpio_t[31:0]),
.gpio1_i (gpio_i[63:32]),
.gpio1_o (gpio_o[63:32]),
.gpio1_t (gpio_t[63:32]),
.iic_main_scl_io (iic_scl),
.iic_main_sda_io (iic_sda),
// .mdio_0_mdc (),
// .mdio_0_mdio_io (1'b0),
.mgt_clk_0_clk_n(USER_MGT_SI570_CLOCK2_N),
.mgt_clk_0_clk_p(USER_MGT_SI570_CLOCK2_P),
// .mgt_ref_clk_0(mgt_ref_clk),
// .sgmii_phyclk_clk_n (phy_clk_n),
// .sgmii_phyclk_clk_p (phy_clk_p),
.phy_rst_n (),
.phy_sd (1'b1),
.ETH_0_RXN (ETH_0_RXN),
.ETH_0_RXP (ETH_0_RXP),
.ETH_0_TXN (ETH_0_TXN),
.ETH_0_TXP (ETH_0_TXP),
.spi_clk_i (spi_clk_mon),
.spi_clk_o (spi_clk_mon),
.spi_csn_i (spi_csn),
.spi_csn_o (spi_csn),
.spi_sdi_i (spi_miso_mon),
.spi_sdo_i (spi_mosi_mon),
.spi_sdo_o (spi_mosi_mon),
.sys_clk_clk_n (USER_SI570_N),
.sys_clk_clk_p (USER_SI570_P),
.sys_rst (sys_rst),
.tx_data_0_n (tx_data_n[0]),
.tx_data_0_p (tx_data_p[0]),
.tx_data_1_n (tx_data_n[1]),
.tx_data_1_p (tx_data_p[1]),
.tx_data_2_n (tx_data_n[2]),
.tx_data_2_p (tx_data_p[2]),
.tx_data_3_n (tx_data_n[3]),
.tx_data_3_p (tx_data_p[3]),
.tx_data_4_n (tx_data_n[4]),
.tx_data_4_p (tx_data_p[4]),
.tx_data_5_n (tx_data_n[5]),
.tx_data_5_p (tx_data_p[5]),
.tx_data_6_n (tx_data_n[6]),
.tx_data_6_p (tx_data_p[6]),
.tx_data_7_n (tx_data_n[7]),
.tx_data_7_p (tx_data_p[7]),
.tx_ref_clk_0 (tx_ref_clk_156),
.tx_ref_clk_4 (tx_ref_clk_156),
.tx_sync_0 (tx_sync),
.tx_sysref_0 (tx_sysref),
.uart_sin (uart_sin),
.uart_sout (uart_sout),
.dac_fifo_bypass (dac_fifo_bypass));
// AD9161/2/4-FMC-EBZ works only in single link,
// The FMC connector instead of SYNC1 has SYSREF connected to it
assign tx_sysref_loc = (DEVICE_CODE == 3) ? tx_sync[1] : tx_sysref;
endmodule
attaching the spi related constraints below:
set_property -dict {PACKAGE_PIN AA1 IOSTANDARD LVCMOS18} [get_ports spi_csn_dac]
set_property -dict {PACKAGE_PIN AB3 IOSTANDARD LVCMOS18} [get_ports spi_csn_clk]
set_property -dict {PACKAGE_PIN AA2 IOSTANDARD LVCMOS18} [get_ports spi_miso]
set_property -dict {PACKAGE_PIN Y1 IOSTANDARD LVCMOS18} [get_ports spi_mosi]
set_property -dict {PACKAGE_PIN Y2 IOSTANDARD LVCMOS18} [get_ports spi_clk]
set_property -dict {PACKAGE_PIN AC3 IOSTANDARD LVCMOS18} [get_ports spi_en]
# For AD916(1,2,3,4)-FMC-EBZ
set_property -dict {PACKAGE_PIN W2 IOSTANDARD LVCMOS18} [get_ports spi_csn_clk2]
# For AD9135-FMC-EBZ, AD9136-FMC-EBZ, AD9144-FMC-EBZ, AD9152-FMC-EBZ, AD9154-FMC-EBZ
set_property -dict {PACKAGE_PIN U5 IOSTANDARD LVCMOS18} [get_ports {dac_ctrl[0]}]
set_property -dict {PACKAGE_PIN U4 IOSTANDARD LVCMOS18} [get_ports {dac_ctrl[3]}]
# For AD9171-FMC-EBZ, AD9172-FMC-EBZ, AD9173-FMC-EBZ
set_property -dict {PACKAGE_PIN AC2 IOSTANDARD LVCMOS18} [get_ports {dac_ctrl[1]}]
set_property -dict {PACKAGE_PIN AC1 IOSTANDARD LVCMOS18} [get_ports {dac_ctrl[2]}]
# For AD916(1,2,3,4)-FMC-EBZ
set_property -dict {PACKAGE_PIN W1 IOSTANDARD LVCMOS18} [get_ports {dac_ctrl[4]}]
It would be really great if someone could guide me on this. Thank you in advance