Post Go back to editing

Issues in ADC DAC loopback for ADRV9002 transceiver for ZCU102 eval board

Thread Summary

The user encountered errors during ADC DAC loopback setup for the ADRV9002 transceiver on the ZCU102 eval board, specifically during initialization calibrations. The final answer directed the user to a previously answered thread on the EngineerZone forum for further troubleshooting and to continue the conversation there. The errors suggest checking for signals on the Rx ports and ensuring correct and synchronized external LOs are applied.
AI Generated Content
Category: Software

Hi,

Currently i am trying to establish a ADC DAC loopback for ADRV9002 transceiver for ZCU102 eval board. For that i have taken the HDL and C files from the github and make changes in it as per the requirement . While doing so i am facing some error messages on launching the project. The issue is very frequent and i got stuck into it. I have attached the prints of the error, kindly look into it and suggest any changes or modification in the project if required. Also let me know if any further information you  required so as to establish the loopback.

regards,

Anurag

Hello
[ERROR]: Error number  3 (0x00000003), Recovery action -101.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_CmdStatus_Wait, in line  671, variable name device.Error message ArmCmdStatusWait() failed due to thrown ARM error. Is device in correct state for calling command?.
[ERROR]: Error number  13315 (0x00003403), Recovery action -2.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/private/src/adrv9001_arm.c, in function adrv9001_ArmCmdErrorHandler, in line  2852, variable name mailboxErrCode.Error message Error occurred during an Init Calibration. Check that no signal is being applied to the Rx ports. Check that correct external LOs are applied, and synchronized,  where appropriate.
[ERROR]: Error number  13315 (0x00003403), Recovery action -2.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/public/src/adi_adrv9001_cals.c, in function adi_adrv9001_cals_InitCals_Run, in line  117, variable name NULL.Error message Error occurred during an Init Calibration. Check that no signal is being applied to the Rx ports. Check that correct external LOs are applied, and synchronized,  where appropriate.
adrv9002_setup, 981: failed with "Error occurred during an Init Calibration. Check that no signal is being applied to the Rx ports. Check that correct external LOs are applied, and synchronized,  where appropriate" (13315)

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.